Overview of axis-specific parameters
Axis data header (kopf.*)
General axis data (kenngr.*)
Functional settings
Gear step dependent parameters (getriebe[i].*)
Parameters for position control
Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)
Parameters for feedforward control
Parameters for drives (antr.*)
Drive type PROFIDRIVE (antr.profibus.*)
General drive parameters
Drive type simulation (antr.simu.*)
Drive type SERCOS (antr.sercos.*)
Drive type CANopen (antr.canopen.*)
Drive type KUKA (antr.dse.*)
Drive type Terminal (antr.terminal.*)
Parameters for drive functions (antr.function[i].*)
Parameterise motion to fixed stop (antr.fixed_stop.*)
Use default value (P-AXIS-00730)
Position lag limit for detection (P-AXIS-00712)
Monitoring window (P-AXIS-00713)
Number of position control cycles (P-AXIS-00714)
Error output on abort (P-AXIS-00715)
Error message if fixed stop is not detected (P-AXIS-00716)
Warning message on reset and detected fixed stop (P-AXIS-00717)
Motor torque at maximum axis acceleration (P-AXIS-00718)
CNC-internal identifier for the drive object (P-AXIS-00719)
Type of communication with drive controller (P-AXIS-00720)
Name of the drive object in the driver amplifier (P-AXIS-00721)
Data type of the data to be transmitted (P-AXIS-00722)
Default value of data element after controller start-up (P-AXIS-00723)
Scaling type of the data element (P-AXIS-00724)
Maximum permissible output value (P-AXIS-00725)
Minimum permissible output value (P-AXIS-00726)
Write/read drive values by bit mask (P-AXIS-00727)
Scaling factor (P-AXIS-00728)
Value of data element during Move to fixed stop (P-AXIS-00729)
Name of the drive object to be read in the driver amplifier (P-AXIS-00731)
Ident is a drive command (P-AXIS-00852)
Use default parameterisation of drive objects (P-AXIS-00821)
Quick stop after detecting the fixed stop (P-AXIS-00762)
Error reaction for missing drive releases (P-AXIS-00763)
Position lag limit for fixed stop detection (P-AXIS-00769)
Minimum time for fixed stop detection (P-AXIS-00770)
Minimum path to activate fixed stop detection (P-AXIS-00771)
Percentage minimum path for fixed stop detection (P-AXIS-00772)
Maximum position change for fixed stop detection (P-AXIS-00773)
Velocity limit for fixed stop detection (P-AXIS-00817)
Default value for torque limit for fixed stop detection (P-AXIS-00818)
During active moving to fixed stop an axis exchange for this axis is allowed (P-AXIS-00831)
Degradation of position lag by interpolation on fixed stop position. (P-AXIS-00832)
Address offset for digital drive types
Use actual speed for speed monitoring (P-AXIS-00779)
Signal for main encoder (P-AXIS-00823)
Signal for secondary encoder (P-AXIS-00824)
Evaluating status bit “Drive follows command values” (P-AXIS-00830)
Relevant bit for touch probe status (P-AXIS-00815)
Parameterising drive data from PLC to drive
Parameterising drive data from PLC to drive
Parameters for manual operation (handbetrieb.*)
Parameters for measurement simulation (meas_simu.*)
Axis-specific filter functions
Parameters for axis specific transformation (trafo.*)
Parameters for path dependent on dynamic weighting (dynamic_weighting.*)
Parameters used by Twincat system manager (twincat.*)
User-defined data (customer.*)
Filter parameters for error handling on axis (error_filter[i].*)
Parameter of the external compensation
Settings for the conveyor tracking functionality (conv_sync.*)
General examples