Overview of axis-specific parameters







Axis data header (kopf.*)







General axis data (kenngr.*)







Functional settings







Gear step dependent parameters (getriebe[i].*)







Parameters for position control







Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)







Parameters for feedforward control







Parameters for drives (antr.*)








Drive type PROFIDRIVE (antr.profibus.*)








General drive parameters









Handling of drive command position (P-AXIS-00123)









Handling of drive actual position (P-AXIS-00122)









Time base for normalisation of velocity (P-AXIS-00207)









Normalisation of the velocity









Delay between command value and actual value (P-AXIS-00191)









Positioning operation mode of an axis (P-AXIS-00320)









Number of the latch input used for edge banding (P-AXIS-00353)









Ignore unknown entries in drive telegram (P-AXIS-00358)









Maximum time delay for disabling drive after a PLC watchdog error (P-AXIS-00367)









Name of the EtherCAT master process (P-AXIS-00372)









Encoder, used for CNC controlled homing (P-AXIS-00388)









Base value for scaling of acceleration feedforward (P-AXIS-00392)









Encoder resolution via feed constant numerator (P-AXIS-00362)









Encoder resolution via feed constant denominator (P-AXIS-00363)









Offset between drive position and CNC position for absolute encoders (P-AXIS-00403)









Factor to coarse encoder resolution (P-AXIS-00405)









EtherCAT-Fieldbus: Number of permissible telegram failures (P-AXIS-00406)









Bit number for control of a DC brake (P-AXIS-00410)









Number of probing input in drive (P-AXIS-00430)









Use of position lag calculated in drive (P-AXIS-00466)









Maximum time for drive reset (P-AXIS-00484)









Drive without support for probing state (P-AXIS-00524)









Activate evaluation of encoder position with additional mask (P-AXIS-00527)









Drive encoder modulo range (P-AXIS-00528)









Mechanical movement distance outside the software limit switches (P-AXIS-00459)









Additional datum to calculate power_state_r










Bit number of additional information for calculation of HLI signal 'power_state_e' (P-AXIS-00709)










Inverting 'Ready for Power' signal (P-AXIS-00710)










Element name of additional information for calculation of HLI signal 'power_state_e' (P-AXIS-00711)









Disabling drive controller for position lag error (P-AXIS-00537)









Disabling drive controller in case of bus error (P-AXIS-00542)









Weighting of velocity feedforward control in drive (P-AXIS-00833)








Drive type simulation (antr.simu.*)








Drive type SERCOS (antr.sercos.*)








Drive type CANopen (antr.canopen.*)








Drive type KUKA (antr.dse.*)








Drive type Terminal (antr.terminal.*)








Parameters for drive functions (antr.function[i].*)








Parameterise motion to fixed stop (antr.fixed_stop.*)








Address offset for digital drive types








Use actual speed for speed monitoring (P-AXIS-00779)








Signal for main encoder (P-AXIS-00823)








Signal for secondary encoder (P-AXIS-00824)








Evaluating status bit “Drive follows command values” (P-AXIS-00830)








Relevant bit for touch probe status (P-AXIS-00815)








Parameterising drive data from PLC to drive








Parameterising drive data from PLC to drive







Parameters for manual operation (handbetrieb.*)







Parameters for measurement simulation (meas_simu.*)







Axis-specific filter functions







Parameters for axis specific transformation (trafo.*)







Parameters for path dependent on dynamic weighting (dynamic_weighting.*)







Parameters used by Twincat system manager (twincat.*)







User-defined data (customer.*)







Filter parameters for error handling on axis (error_filter[i].*)







Parameter of the external compensation







Settings for the conveyor tracking functionality (conv_sync.*)







General examples