Overview of axis-specific parameters
Axis data header (kopf.*)
General axis data (kenngr.*)
Functional settings
Gear step dependent parameters (getriebe[i].*)
Parameters for position control
Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)
Parameters for feedforward control
Parameters for drives (antr.*)
Drive type PROFIDRIVE (antr.profibus.*)
General drive parameters
Handling of drive command position (P-AXIS-00123)
Handling of drive actual position (P-AXIS-00122)
Time base for normalisation of velocity (P-AXIS-00207)
Normalisation of the velocity
Normalisation of the velocity numerator (P-AXIS-00206)
Normalisation of the velocity denominator (P-AXIS-00205)
Normalisation of the velocity
Delay between command value and actual value (P-AXIS-00191)
Positioning operation mode of an axis (P-AXIS-00320)
Number of the latch input used for edge banding (P-AXIS-00353)
Ignore unknown entries in drive telegram (P-AXIS-00358)
Maximum time delay for disabling drive after a PLC watchdog error (P-AXIS-00367)
Name of the EtherCAT master process (P-AXIS-00372)
Encoder, used for CNC controlled homing (P-AXIS-00388)
Base value for scaling of acceleration feedforward (P-AXIS-00392)
Encoder resolution via feed constant numerator (P-AXIS-00362)
Encoder resolution via feed constant denominator (P-AXIS-00363)
Offset between drive position and CNC position for absolute encoders (P-AXIS-00403)
Factor to coarse encoder resolution (P-AXIS-00405)
EtherCAT-Fieldbus: Number of permissible telegram failures (P-AXIS-00406)
Bit number for control of a DC brake (P-AXIS-00410)
Number of probing input in drive (P-AXIS-00430)
Use of position lag calculated in drive (P-AXIS-00466)
Maximum time for drive reset (P-AXIS-00484)
Drive without support for probing state (P-AXIS-00524)
Activate evaluation of encoder position with additional mask (P-AXIS-00527)
Drive encoder modulo range (P-AXIS-00528)
Mechanical movement distance outside the software limit switches (P-AXIS-00459)
Additional datum to calculate power_state_r
Disabling drive controller for position lag error (P-AXIS-00537)
Disabling drive controller in case of bus error (P-AXIS-00542)
Weighting of velocity feedforward control in drive (P-AXIS-00833)
Drive type simulation (antr.simu.*)
Drive type SERCOS (antr.sercos.*)
Drive type CANopen (antr.canopen.*)
Drive type KUKA (antr.dse.*)
Drive type Terminal (antr.terminal.*)
Parameters for drive functions (antr.function[i].*)
Parameterise motion to fixed stop (antr.fixed_stop.*)
Address offset for digital drive types
Use actual speed for speed monitoring (P-AXIS-00779)
Signal for main encoder (P-AXIS-00823)
Signal for secondary encoder (P-AXIS-00824)
Evaluating status bit “Drive follows command values” (P-AXIS-00830)
Relevant bit for touch probe status (P-AXIS-00815)
Parameterising drive data from PLC to drive
Parameterising drive data from PLC to drive
Parameters for manual operation (handbetrieb.*)
Parameters for measurement simulation (meas_simu.*)
Axis-specific filter functions
Parameters for axis specific transformation (trafo.*)
Parameters for path dependent on dynamic weighting (dynamic_weighting.*)
Parameters used by Twincat system manager (twincat.*)
User-defined data (customer.*)
Filter parameters for error handling on axis (error_filter[i].*)
Parameter of the external compensation
Settings for the conveyor tracking functionality (conv_sync.*)
General examples