Overview of axis-specific parameters







Axis data header (kopf.*)







General axis data (kenngr.*)







Functional settings







Gear step dependent parameters (getriebe[i].*)







Parameters for position control







Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)







Parameters for feedforward control







Parameters for drives (antr.*)








Drive type PROFIDRIVE (antr.profibus.*)









Factor for calculation of the position value (P-AXIS-00065)









Slave-life sign limit (P-AXIS-00162)









Activation of velocity command interface (P-AXIS-00260)









Reading absolute position from drive (P-AXIS-00315)









Offset factor for G1_XIST1 (P-AXIS-00316)









Offset factor for absolute value in G1_XIST2 (P-AXIS-00317)









Calculation mode for actual position (P-AXIS-00318)









Offset to the read absolute position of the drive (P-AXIS-00341)









Automatic follow up mode for disabled drive (P-AXIS-00352)









Number of detectable motor revolutions (P-AXIS-00336)









Velocity scaling factor (P-AXIS-00379)









Suppress slave life sign warning (P-AXIS-00462)









Encoder settings for additive encoders (antr.profibus.encoder[i].*)










Reading the encoder's absolute position out of the drive (P-AXIS-00447)










Calculation mode for encoder's actual position (P-AXIS-00448)










Offset from the read absolute position of the encoder (P-AXIS-00449)










Offset factor for absolute value in GX_XIST2 (P-AXIS-00450)










Offset factor for GX_XIST1 (P-AXIS-00451)









Mechanical movement distance outside the software limit switches (P-AXIS-00546)








General drive parameters








Drive type simulation (antr.simu.*)








Drive type SERCOS (antr.sercos.*)








Drive type CANopen (antr.canopen.*)








Drive type KUKA (antr.dse.*)








Drive type Terminal (antr.terminal.*)








Parameters for drive functions (antr.function[i].*)








Parameterise motion to fixed stop (antr.fixed_stop.*)








Address offset for digital drive types








Use actual speed for speed monitoring (P-AXIS-00779)








Signal for main encoder (P-AXIS-00823)








Signal for secondary encoder (P-AXIS-00824)








Evaluating status bit “Drive follows command values” (P-AXIS-00830)








Relevant bit for touch probe status (P-AXIS-00815)








Parameterising drive data from PLC to drive








Parameterising drive data from PLC to drive







Parameters for manual operation (handbetrieb.*)







Parameters for measurement simulation (meas_simu.*)







Axis-specific filter functions







Parameters for axis specific transformation (trafo.*)







Parameters for path dependent on dynamic weighting (dynamic_weighting.*)







Parameters used by Twincat system manager (twincat.*)







User-defined data (customer.*)







Filter parameters for error handling on axis (error_filter[i].*)







Parameter of the external compensation







Settings for the conveyor tracking functionality (conv_sync.*)







General examples