Industrie-PC

 Feldbuskomponenten

 Antriebstechnik


 Servoverstärker


 Dezentrale Servoantriebssysteme


 Rotatorische Servomotoren


 Translatorische Servomotoren


 Planetengetriebe


 Transportsysteme


 Kompakte Antriebstechnik


 Zubehör


 Software



 TE5910 | TC3 Motion Designer - Kurzinbetriebnahme



 AX8000 | Multiachs-Servosystem - Funktionsbeschreibung



 AX5000 | Digital Kompakt Servoverstärker - Funktionsbeschreibung



 AX5000 | Digital compact servo drives - IDN-Beschreibung



 AX5000 | Digital Kompakt Servoverstärker - Diagnosemeldungen



 AX5000 EMV-Handbuch - Version 1.1



 AX5000 Tuning-Guide - Version 1.0



 AX8xxx | Axis module - Diagnostic messages



 AX8xxx | Axis module - Object dictionary



 AX86x0 | Power supply module - Object dictionary



 AX86x0 | Power supply module - Diagnostic messages



 AX8820 | Universal regenerative unit - Diagnostic messages



 AX8820 | Universal regenerative unit - Object Dictionary



 AMP8000 | Distributed servo drives - Diagnostic messages




 Standard-Messages




 Diagmessages of DeviceMainSlot




 Diagmessages of SafetySlot




 Diagmessages of DeviceDebugSlot




 Diagmessages of AxisMainSlot





 0000, No Error





 2340, Short circuit (motor-side)





 2380, Continuous over current (device output side) Phase U





 2381, Continuous over current (device output side) Phase V





 2382, Continuous over current (device output side) Phase W





 2383, Phase U current offset out of range





 2384, Phase V current offset out of range





 2385, Phase W current offset out of range





 2386, Motor brake current offset out of range





 3180, Phase failure motor





 3220, DC link under-voltage





 3280, DC link is not ready





 4310, Drive overtemperature shut down





 5180, Output stage STO active.





 5184, Supply DC link circuit is not ready





 5187, Power supply communication is not established





 5441, Positive limit switch active





 5442, Negative limit switch active





 5443, Loss of the hardware enable





 5444, Loss of the hardware enable (Reaction TorqueOff)





 5445, Fast stop switch active





 54B1, Positive limit switch active





 54B2, Negative limit switch active





 54B3, Fast stop switch active





 5595, Modulo remainder will not be stored.





 589C, Persistent Data Error





 589E, Persistent data memory error. Primary position offset.





 589F, Persistent data memory error. Secondary position offset.





 58A0, Persistent data memory error. Modulo remainder.





 6183, Internal Watchdog Error





 638A, The Axis seems not to be parameterized.





 6390, Factor Group Parameters: Feed constant illegal feed





 6391, Factor Group Parameters: Feed constant illegal shaft revolutions





 6392, Factor Group Parameters: Gear ratio illegal Motor shaft revolutions





 6393, Factor Group Parameters: Gear ratio illegal Driving shaft revolutions





 6394, Factor Group Parameters: Position encoder resolution illegal encoder increments





 6395, Factor Group Parameters: Position encoder resolution illegal motor revolutions





 6396, additional Factor Group Parameters: Feed constant illegal feed





 6397, additional Factor Group Parameters: Feed constant illegal shaft revolutions





 6398, additional Factor Group Parameters: Gear ratio illegal Motor shaft revolutions





 6399, additional Factor Group Parameters: Gear ratio illegal Driving shaft revolutions





 639A, additional Factor Group Parameters: Position encoder resolution illegal encoder increments





 639B, additional Factor Group Parameters: Position encoder resolution illegal motor revolutions





 639C, Velocity factor illegal. A possible Value would be UU/UU.





 639D, Acceleration factor illegal. A possible Value would be UU/UU.





 639E, Scaling index object 0xXX does not fit the Factor group parameters for the first Encoder





 639F, Scaling index object 0xXX does not fit the Factor group parameters for the second Encoder





 63A0, Motor or Primary Feedback changed





 63A1, Secondary Feedback changed





 63A2, Offset position actual value: No position offset existing in source 'encoder memory'





 63A3, Offset additional position actual value: No position offset existing in source 'encoder memory'





 63A4, Offset position actual value: No position offset existing in source 'drive memory'





 63A5, Offset additional position actual value: No position offset existing in source 'drive memory'





 63A6, Jerk factor illegal. A possible Value would be UU/UU.





 63A7, The range UU of the Position range limit is below the minimum accepted value of UU.





 63A8, Position range limit Inc with remainder is not supported for primary feedback.





 63A9, Position range limit Inc with remainder is not supported for secondary feedback.





 63AA, Object 0xXX/XX changed in EtherCAT SafeOP or OP.





 63AB, Offset position actual value: Found an internal encoder postion offset. No other offset can be selected.





 63AC, Offset addtional position actual value: Found an internal encoder postion offset. No other offset can be selected.





 63AE, Modulo calculation primary feedback: No saved data could be loaded





 63AF, Modulo calculation primary feedback: No saved data could be loaded. Remainder Changed.





 63B7, Modulo calculation primary feedback: The absolute range of encoder is too small or incompatible





 7180, Motor brake: Current monitoring error.





 7380, Current sensor motor phase U





 7381, Current sensor motor phase V





 7382, Current sensor motor phase W





 7398, Physical position sensor required





 7399, Simulation feedback module required





 8182, EtherCAT Statemachine shutdown with enabled Axis





 8183, Controlword output cycle counter monitoring





 8184, Dynoutput cycle counter monitoring





 8185, Axis needs an extended fault reset command





 8187, PWM carrier signal PLL not locked to EtherCAT DC SYNC0





 8190, Axis fault reset command is not possible - internal hardware error





 8191, Axis fault reset command is not possible because at least one of the present errors cannot be reset.





 8690, Autotuning command: Out of position range





 8691, Advanced Tuning command: Excitation signal amplitude to high





 8A80, Illegal Modes Of Operation





 8A81, Illegal Modes Of Operation change





 8A82, Error reaction "NC Handling" had a timeout





 A017, Pdo Mapping Error: Object has to be mapped always.





 FF01, Init Timeout





 FF07, Error reaction forced: Torque Off





 FF08, Error reaction forced: Shorted Coils Brake





 FF09, Error reaction forced: Open Loop Ramp





 FF0A, Error reaction forced: Closed Loop Ramp





 FF0B, Error reaction forced: NC handling





 FF0C, Error reaction TorqueOff with emergency brake





 FF0D, Propagated error received, react with Torque Off.





 FF0E, Propagated error received, react with Shorted Coils Brake.





 FF0F, Propagated error received, react with Closed Loop Ramp.





 FF10, Propagated error received, react with NC handling.





 FF11, Error reaction shorted coils brake with emergency brake





 FF12, Error reaction TorqueOff Timeout





 FFFF, Internal Error, Additional Errorcode 0xXX




 Diagmessages of InterpolatorSlot




 Diagmessages of PositionControlSlot




 Diagmessages of VelocityControlSlot




 Diagmessages of BiquadFilterSlot




 Diagmessages of TorqueControlSlot




 Diagmessages of FeedbackSlot




 Diagmessages of MotorSlot




 Diagmessages of AxisDebugSlot



 AMP8000 | Distributed servo drives - Object Dictionary


 Archiv

 TwinCAT 3

 TwinCAT 2

 MX-System

 Branchenlösungen

 Suche

 News

 Home