Overview of axis-specific parameters







Axis data header (kopf.*)







General axis data (kenngr.*)







Functional settings







Gear step dependent parameters (getriebe[i].*)







Parameters for position control








Proportional factor kv for P-positional control (P-AXIS-00099)








Position window for exact stop (P-AXIS-00236)








Position window for rapid movements (P-AXIS-00472)








Activation of position controller-interfaces








Settings for backlash compensation








Settings for temperature compensation








Activate crosstalk compensation (P-AXIS-00789)








Monitoring of axis compensations








Settings for position lag monitoring








Tendency test (P-AXIS-00189)








Settings for dynamic monitoring in position controller








Adaptation of command values








Measurement value adaptation








Quantisation of the measuring system increments (P-AXIS-00323)








Definition of traverse distance between lubrication pulses (P-AXIS-00237)








Settings for axis compensations








Settings for the volumetric compensation (lr_param.vol_comp.*)








Settings for dynamic kv adjustment (getriebe[i].dyn_kv.*)








Parameters for distance control









Enabling of distance control (P-AXIS-00328)









Filtering of sensor values (P-AXIS-00413)









Maximum position offset (P-AXIS-00414)









Maximum velocity (P-AXIS-00415)









Maximum acceleration (P-AXIS-00416)









Maximum permissible change speed of measured distance (P-AXIS-00417)









Reference point offset for control measuring system (P-AXIS-00418)









Upper limit for measuring system (P-AXIS-00419)









Lower limit for measuring system (P-AXIS-00420)









Tolerance band for limits (P-AXIS-00421)









Consideration of distance control in software limit switch monitoring (P-AXIS-00428)









Option: Coupling of distance sensor and motor encoder (P-AXIS-00500)









Option: Adaptive weighting of acceleration (P-AXIS-00501)









Option: Low pass filter (P-AXIS-00506)










Order of the filter (P-AXIS-00507)










Characteristic frequency of a filter (P-AXIS-00508)









Option: Dead time reduction (P-AXIS-00509)









Velocity weighting for the lowering movement (P-AXIS-00533)









Weighting the distance control output values (P-AXIS-00759)









Acceleration weighting for the lowering movement (P-AXIS-00534)









Integral action time of PID controller (P-AXIS-00764)









Derivative action time of PID controller (P-AXIS-00765)









Filter type for smoothing sensor values (P-AXIS-00782)









Uncertainty of measurement values (P-AXIS-00783)









Smoothing factor (P-AXIS-00784)









Tolerance window for control deviation after WAIT command (P-AXIS-00868)









Number of cycles for control deviation after WAIT command (P-AXIS-00869)









Maximum waiting time for waiting condition (P-AXIS-00870)








Position controller dead band (P-AXIS-00395)








Settings for I (Integral) -position control








Improved Position Control (lr_param.improved_position_control.*)








Restoring axis position at controller start (P-AXIS-00761)








Switch over drive type to simulation







Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)







Parameters for feedforward control







Parameters for drives (antr.*)







Parameters for manual operation (handbetrieb.*)







Parameters for measurement simulation (meas_simu.*)







Axis-specific filter functions







Parameters for axis specific transformation (trafo.*)







Parameters for path dependent on dynamic weighting (dynamic_weighting.*)







Parameters used by Twincat system manager (twincat.*)







User-defined data (customer.*)







Filter parameters for error handling on axis (error_filter[i].*)







Parameter of the external compensation







Settings for the conveyor tracking functionality (conv_sync.*)







General examples