Industrial PC
Fieldbus Components
Drive Technology
TwinCAT 3
TwinCAT 2
System Concept
Quick Start
System
System Manager
TX1200 | TwinCAT PLC
TX12xx | TwinCAT NC
NC Basics
TX1250 | NC PTP
TX1260 | NC I
TX1270 | TwinCAT CNC
TX1270 | CNC
Axis Compensation
Axis Commissioning
Axis Parameter
Foreword
Overview of all axis specific parameters
General description
Axis data header (kopf.*)
General axis data (kenngr.*)
Functional settings
Parameters for position control
Proportional factor kv for P-positional control (P-AXIS-00099)
Control window (P-AXIS-00236)
Activation of position controller-interfaces
Activation of display function (P-AXIS-00023)
Activation of (additional) interface for loading application-specific command values (P-AXIS-00091)
Activation of (additional) interface for loading of command and actual values (P-AXIS-00141)
Handling of the loaded position command values (P-AXIS-00322)
Time constant of the PT2-Filter for the additive command value interface (P-AXIS-00438)
Optimized bus access (P-AXIS-00276)
Settings for leadscrew error compensation
Settings for backlash compensation
Settings for temperature compensation
Settings for following error monitoring
Tendency Test (P-AXIS-00189)
Factor for permissible axis velocity (P-AXIS-00407)
Adaptation of command value of drive to the D/A-converter (P-AXIS-00129/ P-AXIS-00128)
Path resolution of the measuring system (P-AXIS-00234/ P-AXIS-00233)
Identific. code for absolute path measurement system (P-AXIS-00014)
Quantization of the measuring system increments (P-AXIS-00323)
Traverse distance (P-AXIS-00237)
Activation of cross compensation (P-AXIS-00047)
Activation of plane compensation (P-AXIS-00174)
Settings for dynamic kv-adjustment (getriebe[i].dyn_kv.*)
Parameter for distance controlled axes (spindle with touch probe)
Position controller deadband (P-AXIS-00395)
Axis peripheral interface parameters for position control (lr_hw[i].*)
Parameters for feedforward control
Parameters for drives (antr.*)
Parameters for manual operation (handbetrieb.*)
Parameters for measurement simulation (meas_simu.*)
Parameters for axis specific filter- function (filter[i].*)
Parameters for axis specific transformation (trafo.*)
Path dependend dynamic weighting(dynamic_weighting.*)
Parameters, that are not being used at the moment
Channel Parameter
Clamp Position Offsets
Diagnosis
External Variables
HLI Interface
Manual Mode Parameter
Programming
Startup List
Tool Data
Zero offsets
System parameters
Kinematic Transformation
MC Platform
PLC library McpPLCopenP1
Function Description
NC Errorcodes
TSxxxx | TwinCAT Supplements
Diagnostics
MX-System
Industry Solutions
General Product Information
Search
News
Home