Industrial PC

Fieldbus Components

Drive Technology

TwinCAT 3

TwinCAT 2


System Concept


Quick Start


System


System Manager


TX1200 | TwinCAT PLC


TX12xx | TwinCAT NC



NC Basics



TX1250 | NC PTP



TX1260 | NC I



TX1270 | TwinCAT CNC




TX1270 | CNC




Axis Compensation




Axis Commissioning




Axis Parameter





Foreword





Overview of all axis specific parameters





General description





Axis data header (kopf.*)





General axis data (kenngr.*)





Functional settings





Parameters for position control






Proportional factor kv for P-positional control (P-AXIS-00099)






Control window (P-AXIS-00236)






Activation of position controller-interfaces






Settings for leadscrew error compensation






Settings for backlash compensation






Settings for temperature compensation






Settings for following error monitoring






Tendency Test (P-AXIS-00189)






Factor for permissible axis velocity (P-AXIS-00407)






Adaptation of command value of drive to the D/A-converter (P-AXIS-00129/ P-AXIS-00128)






Path resolution of the measuring system (P-AXIS-00234/ P-AXIS-00233)






Identific. code for absolute path measurement system (P-AXIS-00014)






Quantization of the measuring system increments (P-AXIS-00323)






Traverse distance (P-AXIS-00237)






Activation of cross compensation (P-AXIS-00047)






Activation of plane compensation (P-AXIS-00174)






Settings for dynamic kv-adjustment (getriebe[i].dyn_kv.*)






Parameter for distance controlled axes (spindle with touch probe)







Enabling of distance control (P-AXIS-00328)







Filtering of sensor values (P-AXIS-00413)







Maximum position offset (P-AXIS-00414)







Maximum velocity (P-AXIS-00415)







Maximum acceleration (P-AXIS-00416)







Maximum permissible change of the measured distance (P-AXIS-00417)







Reference point offset for control measuring system (P-AXIS-00418)







Upper limit for measuring system (P-AXIS-00419)







Lower limit for measuring system (P-AXIS-00420)







Tolerance band for limits (P-AXIS-00421)







Consideration of distance control in software limit switch monitoring (P-AXIS-00428)






Position controller deadband (P-AXIS-00395)





Axis peripheral interface parameters for position control (lr_hw[i].*)





Parameters for feedforward control





Parameters for drives (antr.*)





Parameters for manual operation (handbetrieb.*)





Parameters for measurement simulation (meas_simu.*)





Parameters for axis specific filter- function (filter[i].*)





Parameters for axis specific transformation (trafo.*)





Path dependend dynamic weighting(dynamic_weighting.*)





Parameters, that are not being used at the moment




Channel Parameter




Clamp Position Offsets




Diagnosis




External Variables




HLI Interface




Manual Mode Parameter




Programming




Startup List




Tool Data




Zero offsets




System parameters




Kinematic Transformation




MC Platform




PLC library McpPLCopenP1




Function Description



NC Errorcodes


TSxxxx | TwinCAT Supplements


Diagnostics

MX-System

Industry Solutions

General Product Information

Search

News

Home