Overview of all channel parameters







Description of elements








Configuration of the NC channel.








Configuration of PLC functions









Settings for M functions










Synchronisation types of M functions (P-CHAN-00041)











Examples of synchronisation of M functions












Synchronisation type MOS (without synchronisation)












Synchronisation type MVS_SVS












Synchronisation type MVS_SNS












Synchronisation type MNS_SNS












Synchronisation type MNE_SNS (only for edge banding option)












Synchronisation type MVS_SLM












Synchronisation type MVS_SLP












Without synchronisation MOS_TS












Synchronisation types MET_SVS, MEP_SVS












Synchronisation types MET_MOS, MEP_MOS










Path or time-related pre-output of M functions (P-CHAN-00070)










Axis-specific M functions (P-CHAN-00039)










Time-out and process times of M functions (P-CHAN-00040)









Settings for H functions









Settings for tool change (tool.* or werkzeug.*)









Process time of homing (P-CHAN-00077)









Calculation model for M/H pre-output time (P-CHAN-00209)









Tolerance for deviation with pre-output position of M/H function (P-CHAN-00760)









Residual path/time calculation with M/H pre-output (P-CHAN-00212)









Number of NC blocks at M/H code look ahead (P-CHAN-00274)








Dimensional units and resolutions








Settings for tool management








Settings for edge banding








Settings for measurement








Global program effectiveness of P parameters (P-CHAN-00067)








Single-step operating mode (P-CHAN-00015)








Settings for diameter programming (P-CHAN-00091)








Settings for circle centre point correction and radius compensation








Settings for RESET








Retention of the last axis configuration (P-CHAN-00460)








Preserve zero offsets after reset or program start (P-CHAN-00879)








Preserve tool data after reset or program start (P-CHAN-00880)








Maximum channel override (P-CHAN-00056)








Sampling of override (P-CHAN-00065)








Mode of the override








Operating principle of PLC feed (P-CHAN-00102)








Settings for vector dynamic limits (vector.*)








Configuration of effector coordinate system (ECS)








Tracking a rotary axis








Switch the default feed axis (P-CHAN-00096)








Valid deceleration ramp at FEEDHOLD (P-CHAN-00097)








Switch over the meaning of M functions (P-CHAN-00098)








Effectiveness of tool compensation data (P-CHAN-00100)








Configuration of path axes








Configuration of spindles








Settings for synchronous mode (synchro_data.*)








Parameterisation of the change logging function (aep.*)








Definition of macros (makro_def[i].*)








Settings for tool radius compensation (TRC)








Configuration of syntax check (syn_chk.*)








Parameterisation of kinematic transformations








Default settings at program start (prog_start.*)








Reduction of tangential transition velocity (P-CHAN-00009)








Including jerk in the polynomial (P-CHAN-00110)








Jerk limiting mode at block transition (P-CHAN-00117)








Additional consideration of curvature at block transition (P-CHAN-00245)








Look ahead speed limit (speed_limit_look_ahead.*)








Settings for manual mode








Exclusivity of measuring system programming (P-CHAN-00116)








Exclusivity of axes programming (P-CHAN-00148)








Subroutine call with M6 (P-CHAN-00118)








Subroutine call with D word (P-CHAN-00429)








Subroutine call at program start / MDI








Subroutine call at program end / MDI








Settings for software limit switch (SLS) monitoring








List interpretation with active NC program (P-CHAN-00146)








Adoption of block number when subroutine is called (P-CHAN-00150)








Parameterisation of HSC machining (hsc.*)








Channel synchronisation on axis exchange (P-CHAN-00154)








Channel initialisation with actual values (P-CHAN-00455)








Program name for automatic streaming (P-CHAN-00158)








Modal effect of I/J/K for circle programming (P-CHAN-00159)








Subroutine calls using G functions








Active testing whether axis group is 'in position' (P-CHAN-00173)








Ignore internal stop conditions with rapid contour visualisation (P-CHAN-00183)








Behaviour with axis errors (P-CHAN-00218)








Path-dependent dynamic weighting








Radius-dependent dynamic weighting








Special manual mode data (man_mode.*)








Cycle programming settings








Settings for edge machining (edge_machining.*)








Decoder block ahead limiting








Exact stop with rapid traverse (P-CHAN-00235)








Check exact stop with additive movements (P-CHAN-00486)








Settings for lifting








Settings for robotics








Limiting the path length of motion block (P-CHAN-00457)








Handling of polynomial blocks of zero length (P-CHAN-00254)








Settings for profile tube processing (tube_profile.*)








Optimised polynomial smoothing (P-CHAN-00259)








Configuration of interpolator input disable (P-CHAN-00267)








Settings for forward/backward movement on the path (forward_backward.*)








User-defined data (customer.*)








Encryption of NC programs (P-CHAN-00283)








Settings for independent axes








Jog of path option after block search (P-CHAN-00305)








Checking the license in the clone channel (P-CHAN-00306)








Positioning of modulo axes on shortest path (P-CHAN-00346)








Optimised insertion of #FLUSH CONTINUE (P-CHAN-00341)








Enable 2-path programming (P-CHAN-00261)








Configuration of general display data








Logging of manual block commands








Filter parameters for error handling in the NC channel (error_filter[i].*)








Settings for programming coordinate systems (coordinate_system.*)








Response of G91 with orientation axes (P-CHAN-00332)








Use of axis numbers of master channel (P-CHAN-00282)








Buffering motion blocks to optimise the feed rate profile (P-CHAN-00329)








Units used in PLCopen functions (P-CHAN-00182)








Starting NC programs without initialisation (P-CHAN-00347)








Logical number of a NC channel (P-CHAN-00400)








Settings for throughfeed machining (conveyor_sync.*)








Settings for dynamic contour control (dcc.*)








Settings for surface feed rate (geo_feed_adapt.*)








NC program paths (path[i].*)








Settings for generating debug data (debug.*)








Configuration of channel interface (provide_channel_interface.*)








Settings for 'Time preview' function








Merge short blocks for optimised contouring (P-CHAN-00321)








Contouring method in inch units (P-CHAN-00439)








Unit of constant cutting velocity (P-CHAN-00360)








Synchronisation of PLCopen jobs (P-CHAN-00359)








Orientation interpolation mode (P-CHAN-00417)








Orientation motion with active machining coordinate system (P-CHAN-00858)








Axis-specific orientation of tool length compensation (P-CHAN-00420)








Deactivate feed factor effect (P-CHAN-00422)








Residual time calculation up to trigger mark, residual time look-ahead








Settings for precalculation








Dynamic look-ahead for axis polynomials (P-CHAN-00453)








Memory size for contour machining (P-CHAN-00467)








Real-time cycles








Compatibility for measuring with #CS/Transformation (P-CHAN-00440)








Calculation mode of resulting ramp time with #CS and #TRAFO (P-CHAN-00758)








Tolerance limit for recalculation with dynamic limitation of axis positions (P-CHAN-00751)








Settings for thread tapping








Settings for thread cutting








Parameter for MultiCore








3D distance control (dist_ctrl[i].*)








Defining a load (load[i].*)








Dynamic model








Load model








Suppressing escape motions (P-CHAN-00430)








Retract after error (P-CHAN-00865)








Position requests with active OTC (P-CHAN-00870)








Settings for dynamic limitation of axis positions








Default receiver for #MSG command (P-CHAN-00878)








Calculate zero point offsets with kinematic transformation (P-CHAN-00851)








Enable extended decoder diagnosis data P-CHAN-00881)








Discontinued parameters