Overview of all channel parameters
Description of elements
Configuration of the NC channel.
Decoding
Tool radius compensation
Defining the functionalities for tool radius compensation (P-CHAN-00550)
Maximum number of logged events (P-CHAN-00551)
Defining the type of logged events (P-CHAN-00552)
Conditional enable of the functionalities (P-CHAN-00553)
Condition for enabling the functionalities (P-CHAN-00554)
Path preparation
Interpolation
Configuration of PLC functions
Dimensional units and resolutions
Settings for tool management
Settings for edge banding
Settings for measurement
Global program effectiveness of P parameters (P-CHAN-00067)
Single-step operating mode (P-CHAN-00015)
Settings for diameter programming (P-CHAN-00091)
Settings for circle centre point correction and radius compensation
Settings for RESET
Retention of the last axis configuration (P-CHAN-00460)
Preserve zero offsets after reset or program start (P-CHAN-00879)
Preserve tool data after reset or program start (P-CHAN-00880)
Maximum channel override (P-CHAN-00056)
Sampling of override (P-CHAN-00065)
Mode of the override
Operating principle of PLC feed (P-CHAN-00102)
Settings for vector dynamic limits (vector.*)
Configuration of effector coordinate system (ECS)
Tracking a rotary axis
Switch the default feed axis (P-CHAN-00096)
Valid deceleration ramp at FEEDHOLD (P-CHAN-00097)
Switch over the meaning of M functions (P-CHAN-00098)
Effectiveness of tool compensation data (P-CHAN-00100)
Configuration of path axes
Configuration of spindles
Settings for synchronous mode (synchro_data.*)
Parameterisation of the change logging function (aep.*)
Definition of macros (makro_def[i].*)
Settings for tool radius compensation (TRC)
Configuration of syntax check (syn_chk.*)
Parameterisation of kinematic transformations
Default settings at program start (prog_start.*)
Reduction of tangential transition velocity (P-CHAN-00009)
Including jerk in the polynomial (P-CHAN-00110)
Jerk limiting mode at block transition (P-CHAN-00117)
Additional consideration of curvature at block transition (P-CHAN-00245)
Look ahead speed limit (speed_limit_look_ahead.*)
Settings for manual mode
Exclusivity of measuring system programming (P-CHAN-00116)
Exclusivity of axes programming (P-CHAN-00148)
Subroutine call with M6 (P-CHAN-00118)
Subroutine call with D word (P-CHAN-00429)
Subroutine call at program start / MDI
Subroutine call at program end / MDI
Settings for software limit switch (SLS) monitoring
List interpretation with active NC program (P-CHAN-00146)
Adoption of block number when subroutine is called (P-CHAN-00150)
Parameterisation of HSC machining (hsc.*)
Channel synchronisation on axis exchange (P-CHAN-00154)
Channel initialisation with actual values (P-CHAN-00455)
Program name for automatic streaming (P-CHAN-00158)
Modal effect of I/J/K for circle programming (P-CHAN-00159)
Subroutine calls using G functions
Active testing whether axis group is 'in position' (P-CHAN-00173)
Ignore internal stop conditions with rapid contour visualisation (P-CHAN-00183)
Behaviour with axis errors (P-CHAN-00218)
Path-dependent dynamic weighting
Radius-dependent dynamic weighting
Special manual mode data (man_mode.*)
Cycle programming settings
Settings for edge machining (edge_machining.*)
Decoder block ahead limiting
Exact stop with rapid traverse (P-CHAN-00235)
Check exact stop with additive movements (P-CHAN-00486)
Settings for lifting
Settings for robotics
Limiting the path length of motion block (P-CHAN-00457)
Handling of polynomial blocks of zero length (P-CHAN-00254)
Settings for profile tube processing (tube_profile.*)
Optimised polynomial smoothing (P-CHAN-00259)
Configuration of interpolator input disable (P-CHAN-00267)
Settings for forward/backward movement on the path (forward_backward.*)
User-defined data (customer.*)
Encryption of NC programs (P-CHAN-00283)
Settings for independent axes
Jog of path option after block search (P-CHAN-00305)
Checking the license in the clone channel (P-CHAN-00306)
Positioning of modulo axes on shortest path (P-CHAN-00346)
Optimised insertion of #FLUSH CONTINUE (P-CHAN-00341)
Enable 2-path programming (P-CHAN-00261)
Configuration of general display data
Logging of manual block commands
Filter parameters for error handling in the NC channel (error_filter[i].*)
Settings for programming coordinate systems (coordinate_system.*)
Response of G91 with orientation axes (P-CHAN-00332)
Use of axis numbers of master channel (P-CHAN-00282)
Buffering motion blocks to optimise the feed rate profile (P-CHAN-00329)
Units used in PLCopen functions (P-CHAN-00182)
Starting NC programs without initialisation (P-CHAN-00347)
Logical number of a NC channel (P-CHAN-00400)
Settings for throughfeed machining (conveyor_sync.*)
Settings for dynamic contour control (dcc.*)
Settings for surface feed rate (geo_feed_adapt.*)
NC program paths (path[i].*)
Settings for generating debug data (debug.*)
Configuration of channel interface (provide_channel_interface.*)
Settings for 'Time preview' function
Merge short blocks for optimised contouring (P-CHAN-00321)
Contouring method in inch units (P-CHAN-00439)
Unit of constant cutting velocity (P-CHAN-00360)
Synchronisation of PLCopen jobs (P-CHAN-00359)
Orientation interpolation mode (P-CHAN-00417)
Orientation motion with active machining coordinate system (P-CHAN-00858)
Axis-specific orientation of tool length compensation (P-CHAN-00420)
Deactivate feed factor effect (P-CHAN-00422)
Residual time calculation up to trigger mark, residual time look-ahead
Settings for precalculation
Dynamic look-ahead for axis polynomials (P-CHAN-00453)
Memory size for contour machining (P-CHAN-00467)
Real-time cycles
Compatibility for measuring with #CS/Transformation (P-CHAN-00440)
Calculation mode of resulting ramp time with #CS and #TRAFO (P-CHAN-00758)
Tolerance limit for recalculation with dynamic limitation of axis positions (P-CHAN-00751)
Settings for thread tapping
Settings for thread cutting
Parameter for MultiCore
3D distance control (dist_ctrl[i].*)
Defining a load (load[i].*)
Dynamic model
Load model
Suppressing escape motions (P-CHAN-00430)
Retract after error (P-CHAN-00865)
Position requests with active OTC (P-CHAN-00870)
Settings for dynamic limitation of axis positions
Default receiver for #MSG command (P-CHAN-00878)
Calculate zero point offsets with kinematic transformation (P-CHAN-00851)
Enable extended decoder diagnosis data P-CHAN-00881)
Discontinued parameters