Preface
General and safety instructions
Brief description
Basic principles of programming
Path information
G functions
Switching and supplementary functions (M/H/T)
Velocities (F/E)
NC block numbers (N)
Subroutine techniques
Parameters and parameter calculation (P)
Statements for influencing NC program flow
Smoothing methods
Additional functions
Restoring axis configurations and axis couplings
Axis exchange commands
Dwell time
Flushing NC channel (#FLUSH, #FLUSH CONTINUE, #FLUSH WAIT)
Cross-block comments (#COMMENT BEGIN/END)
Waiting for event (#WAIT FOR)
Adapting minimum radius for tangential feed ((#TANGFEED))
Suppressing offsets (#SUPPRESS OFFSETS)
Settings for measurement
Selecting position preset (#PSET)
Synchronous operation
Messages from the NC program
Jerk limiting slope
Writing and reading SERCOS parameters and commands
Drive parameters (#IDENT)
Non-synchronised write (#IDENT WR)
Non-synchronised read (#IDENT RD)
Synchronised write (#IDENT WR SYN)
SERCOS commands (COMMAND)
Channel synchronisation
Rotate the coordinate system in the plane (#ROTATION ON/OFF)
Automatic axis tracking (C axis tracking) (#CAXTRACK)
User-defined error output (#ERROR)
Time measurement (#TIMER)
Definition of feed axes (#FGROUP, #FGROUP ROT, #FGROUP WAXIS)
Adapt path dynamic limit values (#VECTOR LIMIT ON/OFF)
Defining a minimum block transition velocity (#TRANSVELMIN ON/OFF)
Writing machine data (#MACHINE DATA)
File operations
Monitoring the work space and protection space
Influence forward/backward motion on path
Tool change with active synchronous mode (#FREE TOOL CHANGE)
Locking program areas for single-step mode (#SINGLE STEP)
Programmable path override (#OVERRIDE)
Drive-independent switching of drive functions
Velocity-optimised motion control by segmentation (#SEGMENTATION)
Enlarging/reducing contours (#SCALE ON/OFF))
Punching and nibbling
Controlling edge machining (#EDGE MACHINING)
Switching dynamic weighting (#DYNAMIC WEIGHT)
Weighting of external feedrate (# FF)
Axis clamping and monitoring (#CLAMP MONITORING)
Gantry start-up (#GANTRY ON/OFF)
Position controller-based axis couplings (#GEAR LINK)
Settings for turning functions (# TURN)
Distance to go display in a program section (#DIST TO GO)
Switching over the resolution to the external velocity interface of the PLC (#EDM ON/OFF)
Setting channel options with #CHANNEL SET
Tool geometry compensation (D)
Variables and calculation of variables
Spindle programming
Macroprogramming (# INIT MACRO TAB)
5-Axis functionality
Programming modulo axes
Extended tool programming
Positioning axes
Axis-specific programming
2-path programming
References