Overview of all channel parameters
Description of elements
Configuration of the NC channel.
Configuration of PLC functions
Dimensional units and resolutions
Settings for tool management
Settings for edge banding
Settings for measurement
Global program effectiveness of P parameters (P-CHAN-00067)
Single-step operating mode (P-CHAN-00015)
Settings for diameter programming (P-CHAN-00091)
Settings for circle centre point correction and radius compensation
Settings for RESET
Retention of the last axis configuration (P-CHAN-00460)
Preserve zero offsets after reset or program start (P-CHAN-00879)
Preserve tool data after reset or program start (P-CHAN-00880)
Maximum channel override (P-CHAN-00056)
Sampling of override (P-CHAN-00065)
Mode of the override
Operating principle of PLC feed (P-CHAN-00102)
Settings for vector dynamic limits (vector.*)
Configuration of effector coordinate system (ECS)
Tracking a rotary axis
Switch the default feed axis (P-CHAN-00096)
Valid deceleration ramp at FEEDHOLD (P-CHAN-00097)
Switch over the meaning of M functions (P-CHAN-00098)
Effectiveness of tool compensation data (P-CHAN-00100)
Configuration of path axes
Configuration of spindles
Settings for synchronous mode (synchro_data.*)
Parameterisation of the change logging function (aep.*)
Definition of macros (makro_def[i].*)
Settings for tool radius compensation (TRC)
Configuration of syntax check (syn_chk.*)
Parameterisation of kinematic transformations
Default settings at program start (prog_start.*)
Reduction of tangential transition velocity (P-CHAN-00009)
Including jerk in the polynomial (P-CHAN-00110)
Jerk limiting mode at block transition (P-CHAN-00117)
Additional consideration of curvature at block transition (P-CHAN-00245)
Look ahead speed limit (speed_limit_look_ahead.*)
Settings for manual mode
Exclusivity of measuring system programming (P-CHAN-00116)
Exclusivity of axes programming (P-CHAN-00148)
Subroutine call with M6 (P-CHAN-00118)
Subroutine call with D word (P-CHAN-00429)
Subroutine call at program start / MDI
Subroutine call at program end / MDI
Settings for software limit switch (SLS) monitoring
List interpretation with active NC program (P-CHAN-00146)
Adoption of block number when subroutine is called (P-CHAN-00150)
Parameterisation of HSC machining (hsc.*)
Channel synchronisation on axis exchange (P-CHAN-00154)
Channel initialisation with actual values (P-CHAN-00455)
Program name for automatic streaming (P-CHAN-00158)
Modal effect of I/J/K for circle programming (P-CHAN-00159)
Subroutine calls using G functions
Active testing whether axis group is 'in position' (P-CHAN-00173)
Ignore internal stop conditions with rapid contour visualisation (P-CHAN-00183)
Behaviour with axis errors (P-CHAN-00218)
Path-dependent dynamic weighting
Radius-dependent dynamic weighting
Special manual mode data (man_mode.*)
Cycle programming settings
Settings for edge machining (edge_machining.*)
Decoder block ahead limiting
Exact stop with rapid traverse (P-CHAN-00235)
Check exact stop with additive movements (P-CHAN-00486)
Settings for lifting
Settings for robotics
Limiting the path length of motion block (P-CHAN-00457)
Handling of polynomial blocks of zero length (P-CHAN-00254)
Settings for profile tube processing (tube_profile.*)
Optimised polynomial smoothing (P-CHAN-00259)
Configuration of interpolator input disable (P-CHAN-00267)
Settings for forward/backward movement on the path (forward_backward.*)
User-defined data (customer.*)
Encryption of NC programs (P-CHAN-00283)
Settings for independent axes
Jog of path option after block search (P-CHAN-00305)
Checking the license in the clone channel (P-CHAN-00306)
Positioning of modulo axes on shortest path (P-CHAN-00346)
Optimised insertion of #FLUSH CONTINUE (P-CHAN-00341)
Enable 2-path programming (P-CHAN-00261)
Configuration of general display data
Logging of manual block commands
Filter parameters for error handling in the NC channel (error_filter[i].*)
Settings for programming coordinate systems (coordinate_system.*)
Response of G91 with orientation axes (P-CHAN-00332)
Use of axis numbers of master channel (P-CHAN-00282)
Buffering motion blocks to optimise the feed rate profile (P-CHAN-00329)
Units used in PLCopen functions (P-CHAN-00182)
Starting NC programs without initialisation (P-CHAN-00347)
Logical number of a NC channel (P-CHAN-00400)
Settings for throughfeed machining (conveyor_sync.*)
Settings for dynamic contour control (dcc.*)
Settings for surface feed rate (geo_feed_adapt.*)
NC program paths (path[i].*)
Settings for generating debug data (debug.*)
Configuration of channel interface (provide_channel_interface.*)
Settings for 'Time preview' function
Merge short blocks for optimised contouring (P-CHAN-00321)
Contouring method in inch units (P-CHAN-00439)
Unit of constant cutting velocity (P-CHAN-00360)
Synchronisation of PLCopen jobs (P-CHAN-00359)
Orientation interpolation mode (P-CHAN-00417)
Orientation motion with active machining coordinate system (P-CHAN-00858)
Axis-specific orientation of tool length compensation (P-CHAN-00420)
Deactivate feed factor effect (P-CHAN-00422)
Residual time calculation up to trigger mark, residual time look-ahead
Settings for precalculation
Dynamic look-ahead for axis polynomials (P-CHAN-00453)
Memory size for contour machining (P-CHAN-00467)
Real-time cycles
Compatibility for measuring with #CS/Transformation (P-CHAN-00440)
Calculation mode of resulting ramp time with #CS and #TRAFO (P-CHAN-00758)
Tolerance limit for recalculation with dynamic limitation of axis positions (P-CHAN-00751)
Settings for thread tapping
Settings for thread cutting
Parameter for MultiCore
3D distance control (dist_ctrl[i].*)
Defining a load (load[i].*)
Dynamic model
Load model
Suppressing escape motions (P-CHAN-00430)
Retract after error (P-CHAN-00865)
Position requests with active OTC (P-CHAN-00870)
Settings for dynamic limitation of axis positions
Earlier triggering of braking process (P-CHAN-00873)
Update rate for limit changes (P-CHAN-00874)
Default receiver for #MSG command (P-CHAN-00878)
Calculate zero point offsets with kinematic transformation (P-CHAN-00851)
Enable extended decoder diagnosis data P-CHAN-00881)
Discontinued parameters