Overview of all channel parameters







Description of elements








Configuration of the NC channel.








Configuration of PLC functions








Dimensional units and resolutions








Settings for tool management








Settings for edge banding








Settings for measurement








Global program effectiveness of P parameters (P-CHAN-00067)








Single-step operating mode (P-CHAN-00015)








Settings for diameter programming (P-CHAN-00091)








Settings for circle centre point correction and radius compensation








Settings for RESET








Retention of the last axis configuration (P-CHAN-00460)








Preserve zero offsets after reset or program start (P-CHAN-00879)








Preserve tool data after reset or program start (P-CHAN-00880)








Maximum channel override (P-CHAN-00056)








Sampling of override (P-CHAN-00065)








Mode of the override








Operating principle of PLC feed (P-CHAN-00102)








Settings for vector dynamic limits (vector.*)








Configuration of effector coordinate system (ECS)








Tracking a rotary axis








Switch the default feed axis (P-CHAN-00096)








Valid deceleration ramp at FEEDHOLD (P-CHAN-00097)








Switch over the meaning of M functions (P-CHAN-00098)








Effectiveness of tool compensation data (P-CHAN-00100)








Configuration of path axes








Configuration of spindles









Number of spindles (P-CHAN-00082)









Spindle name within a path compound (P-CHAN-00010)









Machine ID with C axis face machining (P-CHAN-00008)









Definition of main spindle









Spindle data (spindel[i].*)










Spindle name (P-CHAN-00007)










Logical axis number (P-CHAN-00036)










Channel-specific PLC spindle (P-CHAN-00069)










Spindle-specific synchronisation types










Timeout and process time of the spindle function S (P-CHAN-00080)










Timeout and process time of M03 (P-CHAN-00044)










Timeout and process time of M04 (P-CHAN-00046)










Timeout and process time of M05 (P-CHAN-00048)










Timeout and process time of M19 (P-CHAN-00042)










Spindle gear change











Direction of range selection (P-CHAN-00074)











Automatic range selection (P-CHAN-00004)











Table of speed ranges (spindel[i].range_table[j].*)










Identification of an optional spindle (P-CHAN-00415)








Settings for synchronous mode (synchro_data.*)








Parameterisation of the change logging function (aep.*)








Definition of macros (makro_def[i].*)








Settings for tool radius compensation (TRC)








Configuration of syntax check (syn_chk.*)








Parameterisation of kinematic transformations








Default settings at program start (prog_start.*)








Reduction of tangential transition velocity (P-CHAN-00009)








Including jerk in the polynomial (P-CHAN-00110)








Jerk limiting mode at block transition (P-CHAN-00117)








Additional consideration of curvature at block transition (P-CHAN-00245)








Look ahead speed limit (speed_limit_look_ahead.*)








Settings for manual mode








Exclusivity of measuring system programming (P-CHAN-00116)








Exclusivity of axes programming (P-CHAN-00148)








Subroutine call with M6 (P-CHAN-00118)








Subroutine call with D word (P-CHAN-00429)








Subroutine call at program start / MDI








Subroutine call at program end / MDI








Settings for software limit switch (SLS) monitoring








List interpretation with active NC program (P-CHAN-00146)








Adoption of block number when subroutine is called (P-CHAN-00150)








Parameterisation of HSC machining (hsc.*)








Channel synchronisation on axis exchange (P-CHAN-00154)








Channel initialisation with actual values (P-CHAN-00455)








Program name for automatic streaming (P-CHAN-00158)








Modal effect of I/J/K for circle programming (P-CHAN-00159)








Subroutine calls using G functions








Active testing whether axis group is 'in position' (P-CHAN-00173)








Ignore internal stop conditions with rapid contour visualisation (P-CHAN-00183)








Behaviour with axis errors (P-CHAN-00218)








Path-dependent dynamic weighting








Radius-dependent dynamic weighting








Special manual mode data (man_mode.*)








Cycle programming settings








Settings for edge machining (edge_machining.*)








Decoder block ahead limiting








Exact stop with rapid traverse (P-CHAN-00235)








Check exact stop with additive movements (P-CHAN-00486)








Settings for lifting








Settings for robotics








Limiting the path length of motion block (P-CHAN-00457)








Handling of polynomial blocks of zero length (P-CHAN-00254)








Settings for profile tube processing (tube_profile.*)








Optimised polynomial smoothing (P-CHAN-00259)








Configuration of interpolator input disable (P-CHAN-00267)








Settings for forward/backward movement on the path (forward_backward.*)








User-defined data (customer.*)








Encryption of NC programs (P-CHAN-00283)








Settings for independent axes








Jog of path option after block search (P-CHAN-00305)








Checking the license in the clone channel (P-CHAN-00306)








Positioning of modulo axes on shortest path (P-CHAN-00346)








Optimised insertion of #FLUSH CONTINUE (P-CHAN-00341)








Enable 2-path programming (P-CHAN-00261)








Configuration of general display data








Logging of manual block commands








Filter parameters for error handling in the NC channel (error_filter[i].*)








Settings for programming coordinate systems (coordinate_system.*)








Response of G91 with orientation axes (P-CHAN-00332)








Use of axis numbers of master channel (P-CHAN-00282)








Buffering motion blocks to optimise the feed rate profile (P-CHAN-00329)








Units used in PLCopen functions (P-CHAN-00182)








Starting NC programs without initialisation (P-CHAN-00347)








Logical number of a NC channel (P-CHAN-00400)








Settings for throughfeed machining (conveyor_sync.*)








Settings for dynamic contour control (dcc.*)








Settings for surface feed rate (geo_feed_adapt.*)








NC program paths (path[i].*)








Settings for generating debug data (debug.*)








Configuration of channel interface (provide_channel_interface.*)








Settings for 'Time preview' function








Merge short blocks for optimised contouring (P-CHAN-00321)








Contouring method in inch units (P-CHAN-00439)








Unit of constant cutting velocity (P-CHAN-00360)








Synchronisation of PLCopen jobs (P-CHAN-00359)








Orientation interpolation mode (P-CHAN-00417)








Orientation motion with active machining coordinate system (P-CHAN-00858)








Axis-specific orientation of tool length compensation (P-CHAN-00420)








Deactivate feed factor effect (P-CHAN-00422)








Residual time calculation up to trigger mark, residual time look-ahead








Settings for precalculation








Dynamic look-ahead for axis polynomials (P-CHAN-00453)








Memory size for contour machining (P-CHAN-00467)








Real-time cycles








Compatibility for measuring with #CS/Transformation (P-CHAN-00440)








Calculation mode of resulting ramp time with #CS and #TRAFO (P-CHAN-00758)








Tolerance limit for recalculation with dynamic limitation of axis positions (P-CHAN-00751)








Settings for thread tapping








Settings for thread cutting








Parameter for MultiCore








3D distance control (dist_ctrl[i].*)








Defining a load (load[i].*)








Dynamic model








Load model








Suppressing escape motions (P-CHAN-00430)








Retract after error (P-CHAN-00865)








Position requests with active OTC (P-CHAN-00870)








Settings for dynamic limitation of axis positions








Default receiver for #MSG command (P-CHAN-00878)








Calculate zero point offsets with kinematic transformation (P-CHAN-00851)








Enable extended decoder diagnosis data P-CHAN-00881)








Discontinued parameters