Preface







General and safety instructions







Brief description







Basic principles of programming







Path information







G functions







Switching and supplementary functions (M/H/T)







Velocities (F/E)







NC block numbers (N)







Subroutine techniques







Parameters and parameter calculation (P)







Statements for influencing NC program flow







Smoothing methods







Additional functions








Restoring axis configurations and axis couplings








Axis exchange commands









Standard syntax










Requesting axes (#CALL AX)










Releasing axes (#PUT AX, #PUT AX ALL)










Definition of an axis configuration (#SET AX)









Extended syntax








Dwell time








Flushing NC channel (#FLUSH, #FLUSH CONTINUE, #FLUSH WAIT)








Cross-block comments (#COMMENT BEGIN/END)








Waiting for event (#WAIT FOR)








Adapting minimum radius for tangential feed ((#TANGFEED))








Suppressing offsets (#SUPPRESS OFFSETS)








Settings for measurement








Selecting position preset (#PSET)








Synchronous operation








Messages from the NC program








Jerk limiting slope








Writing and reading SERCOS parameters and commands








Channel synchronisation








Rotate the coordinate system in the plane (#ROTATION ON/OFF)








Automatic axis tracking (C axis tracking) (#CAXTRACK)








User-defined error output (#ERROR)








Time measurement (#TIMER)








Definition of feed axes (#FGROUP, #FGROUP ROT, #FGROUP WAXIS)








Adapt path dynamic limit values (#VECTOR LIMIT ON/OFF)








Defining a minimum block transition velocity (#TRANSVELMIN ON/OFF)








Writing machine data (#MACHINE DATA)








File operations








Monitoring the work space and protection space








Influence forward/backward motion on path








Tool change with active synchronous mode (#FREE TOOL CHANGE)








Locking program areas for single-step mode (#SINGLE STEP)








Programmable path override (#OVERRIDE)








Drive-independent switching of drive functions








Velocity-optimised motion control by segmentation (#SEGMENTATION)








Enlarging/reducing contours (#SCALE ON/OFF))








Punching and nibbling








Controlling edge machining (#EDGE MACHINING)








Switching dynamic weighting (#DYNAMIC WEIGHT)








Weighting of external feedrate (# FF)








Axis clamping and monitoring (#CLAMP MONITORING)








Gantry start-up (#GANTRY ON/OFF)








Position controller-based axis couplings (#GEAR LINK)








Settings for turning functions (# TURN)








Distance to go display in a program section (#DIST TO GO)








Switching over the resolution to the external velocity interface of the PLC (#EDM ON/OFF)








Setting channel options with #CHANNEL SET







Tool geometry compensation (D)







Variables and calculation of variables







Spindle programming







Macroprogramming (# INIT MACRO TAB)







5-Axis functionality







Programming modulo axes







Extended tool programming







Positioning axes







Axis-specific programming







2-path programming







References