Overview of axis-specific parameters
Axis data header (kopf.*)
General axis data (kenngr.*)
Functional settings
Gear step dependent parameters (getriebe[i].*)
Parameters for position control
Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)
Parameters for feedforward control
Parameters for drives (antr.*)
Parameters for manual operation (handbetrieb.*)
Parameters for measurement simulation (meas_simu.*)
Axis-specific filter functions
Parameters for axis specific transformation (trafo.*)
Parameters for path dependent on dynamic weighting (dynamic_weighting.*)
Parameters used by Twincat system manager (twincat.*)
User-defined data (customer.*)
Filter parameters for error handling on axis (error_filter[i].*)
Parameter of the external compensation
Settings for the conveyor tracking functionality (conv_sync.*)
General examples
Appendix
Legacy parameters
Activation of (additional) interface for loading application-specific command values (P-AXIS-00091)
Activation of (additional) interface for loading of command and actual values (P-AXIS-00141)
Time constant of the PT2-Filter for the additive command value interface (P-AXIS-00438)
Handling of the loaded position command values as offset (P-AXIS-00322)
Reinitialisation of additional position interface on enable (P-AXIS-00499)
Use default parameters for the drive type (P-AXIS-00746)
Torque limit value (P-AXIS-00342)
Reducing the torque limit for detection (P-AXIS-00343)