Overview of axis-specific parameters
Axis data header (kopf.*)
General axis data (kenngr.*)
Functional settings
Gear step dependent parameters (getriebe[i].*)
Parameters for position control
Proportional factor kv for P-positional control (P-AXIS-00099)
Position window for exact stop (P-AXIS-00236)
Position window for rapid movements (P-AXIS-00472)
Activation of position controller-interfaces
Settings for backlash compensation
Settings for temperature compensation
Activate crosstalk compensation (P-AXIS-00789)
Monitoring of axis compensations
Settings for position lag monitoring
Tendency test (P-AXIS-00189)
Settings for dynamic monitoring in position controller
Adaptation of command values
Adaptation of command value of drive to the drive format (denominator, P-AXIS-00128)
Adaptation of command value of drive to the drive format (numerator, P-AXIS-00129)
Measurement value adaptation
Quantisation of the measuring system increments (P-AXIS-00323)
Definition of traverse distance between lubrication pulses (P-AXIS-00237)
Settings for axis compensations
Settings for the volumetric compensation (lr_param.vol_comp.*)
Settings for dynamic kv adjustment (getriebe[i].dyn_kv.*)
Parameters for distance control
Position controller dead band (P-AXIS-00395)
Settings for I (Integral) -position control
Improved Position Control (lr_param.improved_position_control.*)
Restoring axis position at controller start (P-AXIS-00761)
Switch over drive type to simulation
Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)
Parameters for feedforward control
Parameters for drives (antr.*)
Parameters for manual operation (handbetrieb.*)
Parameters for measurement simulation (meas_simu.*)
Axis-specific filter functions
Parameters for axis specific transformation (trafo.*)
Parameters for path dependent on dynamic weighting (dynamic_weighting.*)
Parameters used by Twincat system manager (twincat.*)
User-defined data (customer.*)
Filter parameters for error handling on axis (error_filter[i].*)
Parameter of the external compensation
Settings for the conveyor tracking functionality (conv_sync.*)
General examples