Industrial PC

Fieldbus Components

Drive Technology


Servo drive



AX8000 | Multi-axis servo system




Operating instructions




Diagmessages for axis modules





Standard-Messages





Diagmessages of DeviceMainSlot





Diagmessages of module SafeMotion





Diagmessages of DeviceDebugSlot





Diagmessages of AxisMainSlot






0000, No Error






2340, Short circuit (motor-side)






2380, Continuous over current (device output side) Phase U






2381, Continuous over current (device output side) Phase V






2382, Continuous over current (device output side) Phase W






2383, Phase U current offset out of range






2384, Phase V current offset out of range






2385, Phase W current offset out of range






2386, Motor brake current offset out of range






3180, Phase failure motor






3220, DC link under-voltage






3280, DC link is not ready






4310, Drive overtemperature shut down






5180, Output stage STO active.






5184, Supply DC link circuit is not ready






5187, Power supply communication is not established






5441, Positive limit switch active






5442, Negative limit switch active






5443, Loss of the hardware enable






5444, Loss of the hardware enable (Reaction TorqueOff)






5445, Fast stop switch active






54B1, Positive limit switch active






54B2, Negative limit switch active






54B3, Fast stop switch active






5595, Modulo remainder will not be stored.






589C, Persistent Data Error






589E, Persistent data memory error. Primary position offset.






589F, Persistent data memory error. Secondary position offset.






58A0, Persistent data memory error. Modulo remainder.






6183, Internal Watchdog Error






638A, The Axis seems not to be parameterized.






6390, Factor Group Parameters: Feed constant illegal feed






6391, Factor Group Parameters: Feed constant illegal shaft revolutions






6392, Factor Group Parameters: Gear ratio illegal Motor shaft revolutions






6393, Factor Group Parameters: Gear ratio illegal Driving shaft revolutions






6394, Factor Group Parameters: Position encoder resolution illegal encoder increments






6395, Factor Group Parameters: Position encoder resolution illegal motor revolutions






6396, additional Factor Group Parameters: Feed constant illegal feed






6397, additional Factor Group Parameters: Feed constant illegal shaft revolutions






6398, additional Factor Group Parameters: Gear ratio illegal Motor shaft revolutions






6399, additional Factor Group Parameters: Gear ratio illegal Driving shaft revolutions






639A, additional Factor Group Parameters: Position encoder resolution illegal encoder increments






639B, additional Factor Group Parameters: Position encoder resolution illegal motor revolutions






639C, Velocity factor illegal. A possible Value would be UU/UU.






639D, Acceleration factor illegal. A possible Value would be UU/UU.






639E, Scaling index object 0xXX does not fit the Factor group parameters for the first Encoder






639F, Scaling index object 0xXX does not fit the Factor group parameters for the second Encoder






63A0, Motor or Primary Feedback changed






63A1, Secondary Feedback changed






63A2, Offset position actual value: No position offset existing in source 'encoder memory'






63A3, Offset additional position actual value: No position offset existing in source 'encoder memory'






63A4, Offset position actual value: No position offset existing in source 'drive memory'






63A5, Offset additional position actual value: No position offset existing in source 'drive memory'






63A6, Jerk factor illegal. A possible Value would be UU/UU.






63A7, The range UU of the Position range limit is below the minimum accepted value of UU.






63A8, Position range limit Inc with remainder is not supported for primary feedback.






63A9, Position range limit Inc with remainder is not supported for secondary feedback.






63AA, Object 0xXX/XX changed in EtherCAT SafeOP or OP.






63AB, Offset position actual value: Found an internal encoder postion offset. No other offset can be selected.






63AC, Offset addtional position actual value: Found an internal encoder postion offset. No other offset can be selected.






63AE, Modulo calculation primary feedback: No saved data could be loaded






63AF, Modulo calculation primary feedback: No saved data could be loaded. Remainder Changed.






63B7, Modulo calculation primary feedback: The absolute range of encoder is too small or incompatible






7180, Motor brake: Current monitoring error.






7380, Current sensor motor phase U






7381, Current sensor motor phase V






7382, Current sensor motor phase W






7398, Physical position sensor required






7399, Simulation feedback module required






8182, EtherCAT Statemachine shutdown with enabled Axis






8183, Controlword output cycle counter monitoring






8184, Dynoutput cycle counter monitoring






8185, Axis needs an extended fault reset command






8187, PWM carrier signal PLL not locked to EtherCAT DC SYNC0






8190, Axis fault reset command is not possible - internal hardware error






8191, Axis fault reset command is not possible because at least one of the present errors cannot be reset.






8690, Autotuning command: Out of position range






8691, Advanced Tuning command: Excitation signal amplitude to high






8A80, Illegal Modes Of Operation






8A81, Illegal Modes Of Operation change






8A82, Error reaction "NC Handling" had a timeout






A017, Pdo Mapping Error: Object has to be mapped always.






FF01, Init Timeout






FF07, Error reaction forced: Torque Off






FF08, Error reaction forced: Shorted Coils Brake






FF09, Error reaction forced: Open Loop Ramp






FF0A, Error reaction forced: Closed Loop Ramp






FF0B, Error reaction forced: NC handling






FF0C, Error reaction TorqueOff with emergency brake






FF0D, Propagated error received, react with Torque Off.






FF0E, Propagated error received, react with Shorted Coils Brake.






FF0F, Propagated error received, react with Closed Loop Ramp.






FF10, Propagated error received, react with NC handling.






FF11, Error reaction shorted coils brake with emergency brake






FF12, Error reaction TorqueOff Timeout






FFFF, Internal Error, Additional Errorcode 0xXX





Diagmessages of InterpolatorSlot





Diagmessages of PositionControlSlot





Diagmessages of VelocityControlSlot





Diagmessages of BiquadFilterSlot





Diagmessages of TorqueControlSlot





Diagmessages of FeedbackSlot





Diagmessages of MotorSlot





Diagmessages of AxisDebugSlot




Object dictionary




Diagmessages for power supply modules




Object dictionary for power supply modules



AX5000 | Digital Compact Servo Drive



AX1000 | Economy servo drive


Variable frequency drive


Distributed drive systems


Rotary servomotors


Translatory servomotors


Planetary gears


XTS | Linear product transport


XPlanar | Planar motor system


Compact drive technology


Accessories


Software


Archive

TwinCAT 3

TwinCAT 2

MX-System

Industry Solutions

General Product Information

Search

News

Home