Standard-Messages
Diagmessages of DeviceMainSlot
Diagmessages of SafetySlot
Diagmessages of DeviceDebugSlot
Diagmessages of AxisMainSlot
Diagmessages of InterpolatorSlot
Diagmessages of PositionControlSlot
Diagmessages of VelocityControlSlot
Diagmessages of BiquadFilterSlot
Diagmessages of TorqueControlSlot
2330, Earth leakage (motor-side)
2390, Amplifier overload utilization
3181, Phase frequency (motor-side) raised above 600 Hz
3182, Velocity actual Value raised above the max channel accepted velocity
6320, Parameter error in object 0xXX/XX
6388, Parameter Torque Control: The value in object 0xXX/XX is higher than the motor peak current (0xXX/XX).
6389, Parameter Torque Control: The value in object 0xXX/XX is higher than the configured peak current (0xXX/XX).
638F, Parameter Torque Control: The value in Object 0xXX/XX is higher than the Motor maximum voltage slope (0xXX/XX).
63AD, Motor torque/ force characteristic is not valid for internal calculation.
63B6, Parameter Torque Control: Invalid device total output current sum
FFFF, Internal Error, Additional Errorcode 0xXX
Diagmessages of FeedbackSlot
Diagmessages of MotorSlot
Diagmessages of AxisDebugSlot
AMP8000 | Distributed servo drives - Object Dictionary
Archive
TwinCAT 3
TwinCAT 2
MX-System
Industry Solutions
General Product Information
Search
News
Home