Overview of axis-specific parameters







Axis data header (kopf.*)







General axis data (kenngr.*)







Functional settings







Gear step dependent parameters (getriebe[i].*)







Parameters for position control








Proportional factor kv for P-positional control (P-AXIS-00099)








Position window for exact stop (P-AXIS-00236)








Position window for rapid movements (P-AXIS-00472)








Activation of position controller-interfaces








Settings for backlash compensation








Settings for temperature compensation








Activate crosstalk compensation (P-AXIS-00789)








Monitoring of axis compensations








Settings for position lag monitoring








Tendency test (P-AXIS-00189)








Settings for dynamic monitoring in position controller








Adaptation of command values








Measurement value adaptation








Quantisation of the measuring system increments (P-AXIS-00323)








Definition of traverse distance between lubrication pulses (P-AXIS-00237)








Settings for axis compensations








Settings for the volumetric compensation (lr_param.vol_comp.*)








Settings for dynamic kv adjustment (getriebe[i].dyn_kv.*)








Parameters for distance control








Position controller dead band (P-AXIS-00395)








Settings for I (Integral) -position control









Integral time Tn for I-position control (P-AXIS-00495)









Maximum output for I-position control (P-AXIS-00496)









Switch on delay for I-position control (P-AXIS-00497)









Clear Integrator if drive is switched off (P-AXIS-00498)








Improved Position Control (lr_param.improved_position_control.*)








Restoring axis position at controller start (P-AXIS-00761)








Switch over drive type to simulation







Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)







Parameters for feedforward control







Parameters for drives (antr.*)







Parameters for manual operation (handbetrieb.*)







Parameters for measurement simulation (meas_simu.*)







Axis-specific filter functions







Parameters for axis specific transformation (trafo.*)







Parameters for path dependent on dynamic weighting (dynamic_weighting.*)







Parameters used by Twincat system manager (twincat.*)







User-defined data (customer.*)







Filter parameters for error handling on axis (error_filter[i].*)







Parameter of the external compensation







Settings for the conveyor tracking functionality (conv_sync.*)







General examples