Overview of axis-specific parameters







Axis data header (kopf.*)







General axis data (kenngr.*)







Functional settings







Gear step dependent parameters (getriebe[i].*)








Gear step number (P-AXIS-00135)








Gear change position (P-AXIS-00078)








Index for hardware specific parameter set (P-AXIS-00054)








Load inertia (P-AXIS-00391)








Dynamic characteristic values









Parameter for linear velocity profile (getriebe[i].lslope_profil.*)









Parameter for non-linear velocity profile (getriebe[i].slope_profil.*)










Acceleration at machining feed (P-AXIS-00001)










Deceleration at machining feed (P-AXIS-00002)










Ramp time for acceleration up-gradation (P-AXIS-00196)










Ramp time for acceleration down-gradation (P-AXIS-00195)










Ramp time for deceleration up-gradation (P-AXIS-00198)










Ramp time for deceleration down-gradation (P-AXIS-00197)










Acceleration at rapid movement (P-AXIS-00004)










Ramp time at rapid movement (P-AXIS-00200)










Deceleration at feedhold (P-AXIS-00053)










Ramp time at feedhold (P-AXIS-00081)









Effective acceleration profile (P-AXIS-00270)









Rapid mode velocity (P-AXIS-00209)









Gearbox ratio numerator/denominator








Permissible axis dynamics (getriebe[i].dynamik.*)








Characteristic curve-controlled acceleration (getriebe[i].beschl_kennlinie.*)








Maximum axis torque (P-AXIS-00798)








First coefficient of the friction model (P-AXIS-00804)








Inertia of the drive (P-AXIS-00828)







Parameters for position control







Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)







Parameters for feedforward control







Parameters for drives (antr.*)







Parameters for manual operation (handbetrieb.*)







Parameters for measurement simulation (meas_simu.*)







Axis-specific filter functions







Parameters for axis specific transformation (trafo.*)







Parameters for path dependent on dynamic weighting (dynamic_weighting.*)







Parameters used by Twincat system manager (twincat.*)







User-defined data (customer.*)







Filter parameters for error handling on axis (error_filter[i].*)







Parameter of the external compensation







Settings for the conveyor tracking functionality (conv_sync.*)







General examples