Overview of axis-specific parameters
Axis data header (kopf.*)
General axis data (kenngr.*)
Functional settings
Gear step dependent parameters (getriebe[i].*)
Gear step number (P-AXIS-00135)
Gear change position (P-AXIS-00078)
Index for hardware specific parameter set (P-AXIS-00054)
Load inertia (P-AXIS-00391)
Dynamic characteristic values
Parameter for linear velocity profile (getriebe[i].lslope_profil.*)
Acceleration of step 1 (P-AXIS-00011)
Acceleration of step 2 (P-AXIS-00012)
Deceleration of step 1 (P-AXIS-00282)
Deceleration of step 2 (P-AXIS-00283)
Changeover speed (P-AXIS-00221)
Acceleration of step 1 in rapid mode (P-AXIS-00005)
Acceleration of step 2 in rapid mode (P-AXIS-00006)
Deceleration of step 1 in rapid mode (P-AXIS-00280)
Deceleration of step 2 in rapid mode (P-AXIS-00281)
Changeover speed in rapid mode (P-AXIS-00211)
Deceleration at feedhold (P-AXIS-00024)
Parameter for non-linear velocity profile (getriebe[i].slope_profil.*)
Effective acceleration profile (P-AXIS-00270)
Rapid mode velocity (P-AXIS-00209)
Gearbox ratio numerator/denominator
Permissible axis dynamics (getriebe[i].dynamik.*)
Characteristic curve-controlled acceleration (getriebe[i].beschl_kennlinie.*)
Maximum axis torque (P-AXIS-00798)
First coefficient of the friction model (P-AXIS-00804)
Inertia of the drive (P-AXIS-00828)
Parameters for position control
Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)
Parameters for feedforward control
Parameters for drives (antr.*)
Parameters for manual operation (handbetrieb.*)
Parameters for measurement simulation (meas_simu.*)
Axis-specific filter functions
Parameters for axis specific transformation (trafo.*)
Parameters for path dependent on dynamic weighting (dynamic_weighting.*)
Parameters used by Twincat system manager (twincat.*)
User-defined data (customer.*)
Filter parameters for error handling on axis (error_filter[i].*)
Parameter of the external compensation
Settings for the conveyor tracking functionality (conv_sync.*)
General examples