Diagmessages




Standard-Messages




Diagmessages of DeviceMainSlot




Diagmessages of SafetySlot




Diagmessages of DeviceDebugSlot




Diagmessages of AxisMainSlot




Diagmessages of InterpolatorSlot




Diagmessages of PositionControlSlot




Diagmessages of VelocityControlSlot




Diagmessages of BiquadFilterSlot




Diagmessages of TorqueControlSlot





2330, Earth leakage (motor-side)





2390, Amplifier overload utilization





3181, Phase frequency (motor-side) raised above 600 Hz





3182, Velocity actual Value raised above the max channel accepted velocity





6320, Parameter error in object 0xXX/XX





6388, Parameter Torque Control: The value in object 0xXX/XX is higher than the motor peak current (0xXX/XX).





6389, Parameter Torque Control: The value in object 0xXX/XX is higher than the configured peak current (0xXX/XX).





638F, Parameter Torque Control: The value in Object 0xXX/XX is higher than the Motor maximum voltage slope (0xXX/XX).





63AD, Motor torque/ force characteristic is not valid for internal calculation.





63B6, Parameter Torque Control: Invalid device total output current sum





FFFF, Internal Error, Additional Errorcode 0xXX




Diagmessages of FeedbackSlot




Diagmessages of MotorSlot




Diagmessages of AxisDebugSlot



Objektbeschreibung


Archiv

TwinCAT 3

TwinCAT 2

MX-System

Branchenlösungen

Allgemeine Produktinformationen

Suche

News

Home