Standard-Messages




Diagmessages of DeviceMainSlot




Diagmessages of module SafeMotion




Diagmessages of DeviceDebugSlot




Diagmessages of AxisMainSlot





0000, No Error





2340, Short circuit (motor-side)





2380, Continuous over current (device output side) Phase U





2381, Continuous over current (device output side) Phase V





2382, Continuous over current (device output side) Phase W





2383, Phase U current offset out of range





2384, Phase V current offset out of range





2385, Phase W current offset out of range





2386, Motor brake current offset out of range





3180, Phase failure motor





3220, DC link under-voltage





3280, DC link is not ready





4310, Drive overtemperature shut down





5180, Output stage STO active.





5184, Supply DC link circuit is not ready





5187, Power supply communication is not established





5441, Positive limit switch active





5442, Negative limit switch active





5443, Loss of the hardware enable





5444, Loss of the hardware enable (Reaction TorqueOff)





5445, Fast stop switch active





54B1, Positive limit switch active





54B2, Negative limit switch active





54B3, Fast stop switch active





5595, Modulo remainder will not be stored.





589C, Persistent Data Error





589E, Persistent data memory error. Primary position offset.





589F, Persistent data memory error. Secondary position offset.





58A0, Persistent data memory error. Modulo remainder.





6183, Internal Watchdog Error





638A, The Axis seems not to be parameterized.





6390, Factor Group Parameters: Feed constant illegal feed





6391, Factor Group Parameters: Feed constant illegal shaft revolutions





6392, Factor Group Parameters: Gear ratio illegal Motor shaft revolutions





6393, Factor Group Parameters: Gear ratio illegal Driving shaft revolutions





6394, Factor Group Parameters: Position encoder resolution illegal encoder increments





6395, Factor Group Parameters: Position encoder resolution illegal motor revolutions





6396, additional Factor Group Parameters: Feed constant illegal feed





6397, additional Factor Group Parameters: Feed constant illegal shaft revolutions





6398, additional Factor Group Parameters: Gear ratio illegal Motor shaft revolutions





6399, additional Factor Group Parameters: Gear ratio illegal Driving shaft revolutions





639A, additional Factor Group Parameters: Position encoder resolution illegal encoder increments





639B, additional Factor Group Parameters: Position encoder resolution illegal motor revolutions





639C, Velocity factor illegal. A possible Value would be UU/UU.





639D, Acceleration factor illegal. A possible Value would be UU/UU.





639E, Scaling index object 0xXX does not fit the Factor group parameters for the first Encoder





639F, Scaling index object 0xXX does not fit the Factor group parameters for the second Encoder





63A0, Motor or Primary Feedback changed





63A1, Secondary Feedback changed





63A2, Offset position actual value: No position offset existing in source 'encoder memory'





63A3, Offset additional position actual value: No position offset existing in source 'encoder memory'





63A4, Offset position actual value: No position offset existing in source 'drive memory'





63A5, Offset additional position actual value: No position offset existing in source 'drive memory'





63A6, Jerk factor illegal. A possible Value would be UU/UU.





63A7, The range UU of the Position range limit is below the minimum accepted value of UU.





63A8, Position range limit Inc with remainder is not supported for primary feedback.





63A9, Position range limit Inc with remainder is not supported for secondary feedback.





63AA, Object 0xXX/XX changed in EtherCAT SafeOP or OP.





63AB, Offset position actual value: Found an internal encoder postion offset. No other offset can be selected.





63AC, Offset addtional position actual value: Found an internal encoder postion offset. No other offset can be selected.





63AE, Modulo calculation primary feedback: No saved data could be loaded





63AF, Modulo calculation primary feedback: No saved data could be loaded. Remainder Changed.





63B7, Modulo calculation primary feedback: The absolute range of encoder is too small or incompatible





7180, Motor brake: Current monitoring error.





7380, Current sensor motor phase U





7381, Current sensor motor phase V





7382, Current sensor motor phase W





7398, Physical position sensor required





7399, Simulation feedback module required





8182, EtherCAT Statemachine shutdown with enabled Axis





8183, Controlword output cycle counter monitoring





8184, Dynoutput cycle counter monitoring





8185, Axis needs an extended fault reset command





8187, PWM carrier signal PLL not locked to EtherCAT DC SYNC0





8190, Axis fault reset command is not possible - internal hardware error





8191, Axis fault reset command is not possible because at least one of the present errors cannot be reset.





8690, Autotuning command: Out of position range





8691, Advanced Tuning command: Excitation signal amplitude to high





8A80, Illegal Modes Of Operation





8A81, Illegal Modes Of Operation change





8A82, Error reaction "NC Handling" had a timeout





A017, Pdo Mapping Error: Object has to be mapped always.





FF01, Init Timeout





FF07, Error reaction forced: Torque Off





FF08, Error reaction forced: Shorted Coils Brake





FF09, Error reaction forced: Open Loop Ramp





FF0A, Error reaction forced: Closed Loop Ramp





FF0B, Error reaction forced: NC handling





FF0C, Error reaction TorqueOff with emergency brake





FF0D, Propagated error received, react with Torque Off.





FF0E, Propagated error received, react with Shorted Coils Brake.





FF0F, Propagated error received, react with Closed Loop Ramp.





FF10, Propagated error received, react with NC handling.





FF11, Error reaction shorted coils brake with emergency brake





FF12, Error reaction TorqueOff Timeout





FFFF, Internal Error, Additional Errorcode 0xXX




Diagmessages of InterpolatorSlot




Diagmessages of PositionControlSlot




Diagmessages of VelocityControlSlot




Diagmessages of BiquadFilterSlot




Diagmessages of TorqueControlSlot




Diagmessages of FeedbackSlot




Diagmessages of MotorSlot




Diagmessages of AxisDebugSlot



Objektbeschreibung für Achsmodule



Objektbeschreibung für Einspeisemodule



Diagmessages für Einspeisemodule



Diagmessages für AX8820



Objektbeschreibung für AX8820



Diagmessages



Objektbeschreibung


Archiv

TwinCAT 3

TwinCAT 2

MX-System

Branchenlösungen

Allgemeine Produktinformationen

Suche

News

Home