Overview of axis-specific parameters
Axis data header (kopf.*)
General axis data (kenngr.*)
Functional settings
Special settings for rotary axes
Settings for modulo calculation for rotary axis
Special settings for spindles
Restriction of direction of rotation (P-AXIS-00224)
Definition of preferred direction of spindle rotation (P-AXIS-00031)
Speed-value attained - tolerance band (P-AXIS-00217)
Dynamic spindle speed monitoring
Upper tolerance band of dynamic speed monitoring (P-AXIS-00838)
Lower tolerance band of dynamic speed monitoring (P-AXIS-00839)
Upper speed of dynamic speed monitoring (P-AXIS-00840)
Limiting velocity for the measurement system (P-AXIS-00220)
Limit for spindle speed 'zero' (P-AXIS-00216)
Reverse of sign for setpoint and actual value (P-AXIS-00159)
Switch to velocity controlled mode (P-AXIS-00265)
Switch back to position control (P-AXIS-00266)
Use actual velocity for revolution monitoring (P-AXIS-00519)
Output time M19 for positioning the spindle (P-AXIS-00523)
Checking commanded spindle speed versus permissible tool speed limits (P-AXIS-00474)
Weighting of velocity feedforward control (P-AXIS-00766)
Velocity limit for switching to velocity controlled mode (P-AXIS-00767)
Velocity limit for switching back to position control (P-AXIS-00768)
Delay time for error message suppression with spindle tool revolution monitoring (P-AXIS-00787)
Limit velocity for delay with spindle tool revolution monitoring (P-AXIS-00788)
Settings for turning functionality
Settings for homing
Settings for software limit switch (SLS) monitoring
Settings for measurement
Activation of edge banding (P-AXIS-00098)
Gantry mode
Monitoring of axis collision
Tracking mode
Gear data
Settings for SAI (Single Axis Interpolation)
Velocity monitoring
Behaviour when enabling the drive controller
Tolerance window for IIR axis filter (P-AXIS-00351)
Tolerance window for IIR axis filter after feedhold (P-AXIS-00780)
Settings for velocity override
Settings for feed rate influencing
Reduced speed
Torque configuration
Gear couplings
Interpolation of tracked axes in inserted TRC blocks (P-AXIS-00427)
Axis specific dynamic monitoring during interpolation
Suppress stop of spindle axis during channel reset (P-AXIS-00455)
Enabling PLCopen interface of a channel axis (P-AXIS-00457)
Collision monitoring during oscillation (P-AXIS-00485)
Inversion of spindle rotation direction for spindle M-functions M3/M4 (P-AXIS-00490)
Delay filter acts only on command positions (P-AXIS-00513)
Enabling of IPO-LR interface after axis release (P-AXIS-00483)
Setting of 'in position' for position controller generated axis movements (P-AXIS-00458)
Settings for drive controllers
Dynamic limits with tool gear (P-AXIS-00786)
Number of bits for command value (P-AXIS-00816)
Gear step dependent parameters (getriebe[i].*)
Parameters for position control
Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)
Parameters for feedforward control
Parameters for drives (antr.*)
Parameters for manual operation (handbetrieb.*)
Parameters for measurement simulation (meas_simu.*)
Axis-specific filter functions
Parameters for axis specific transformation (trafo.*)
Parameters for path dependent on dynamic weighting (dynamic_weighting.*)
Parameters used by Twincat system manager (twincat.*)
User-defined data (customer.*)
Filter parameters for error handling on axis (error_filter[i].*)
Parameter of the external compensation
Settings for the conveyor tracking functionality (conv_sync.*)
General examples