Overview of axis-specific parameters







Axis data header (kopf.*)







General axis data (kenngr.*)







Functional settings








Special settings for rotary axes








Settings for homing








Settings for software limit switch (SLS) monitoring








Settings for measurement








Activation of edge banding (P-AXIS-00098)








Gantry mode








Monitoring of axis collision








Tracking mode








Gear data








Settings for SAI (Single Axis Interpolation)








Velocity monitoring









Velocity limit during active monitoring of current velocity (P-AXIS-00311)









Activation of speed monitoring (P-AXIS-00312)









Activation of feed enable via PLC (P-AXIS-00313)









Speed monitoring during torque limitation (P-AXIS-00314)








Behaviour when enabling the drive controller








Tolerance window for IIR axis filter (P-AXIS-00351)








Tolerance window for IIR axis filter after feedhold (P-AXIS-00780)








Settings for velocity override








Settings for feed rate influencing








Reduced speed








Torque configuration








Gear couplings








Interpolation of tracked axes in inserted TRC blocks (P-AXIS-00427)








Axis specific dynamic monitoring during interpolation








Suppress stop of spindle axis during channel reset (P-AXIS-00455)








Enabling PLCopen interface of a channel axis (P-AXIS-00457)








Collision monitoring during oscillation (P-AXIS-00485)








Inversion of spindle rotation direction for spindle M-functions M3/M4 (P-AXIS-00490)








Delay filter acts only on command positions (P-AXIS-00513)








Enabling of IPO-LR interface after axis release (P-AXIS-00483)








Setting of 'in position' for position controller generated axis movements (P-AXIS-00458)








Settings for drive controllers








Dynamic limits with tool gear (P-AXIS-00786)








Number of bits for command value (P-AXIS-00816)







Gear step dependent parameters (getriebe[i].*)







Parameters for position control







Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)







Parameters for feedforward control







Parameters for drives (antr.*)







Parameters for manual operation (handbetrieb.*)







Parameters for measurement simulation (meas_simu.*)







Axis-specific filter functions







Parameters for axis specific transformation (trafo.*)







Parameters for path dependent on dynamic weighting (dynamic_weighting.*)







Parameters used by Twincat system manager (twincat.*)







User-defined data (customer.*)







Filter parameters for error handling on axis (error_filter[i].*)







Parameter of the external compensation







Settings for the conveyor tracking functionality (conv_sync.*)







General examples