Overview of axis-specific parameters







Axis data header (kopf.*)







General axis data (kenngr.*)







Functional settings








Special settings for rotary axes








Settings for homing








Settings for software limit switch (SLS) monitoring








Settings for measurement








Activation of edge banding (P-AXIS-00098)








Gantry mode








Monitoring of axis collision








Tracking mode








Gear data








Settings for SAI (Single Axis Interpolation)








Velocity monitoring








Behaviour when enabling the drive controller








Tolerance window for IIR axis filter (P-AXIS-00351)








Tolerance window for IIR axis filter after feedhold (P-AXIS-00780)








Settings for velocity override








Settings for feed rate influencing








Reduced speed








Torque configuration









Torque offset (P-AXIS-00324)









Numerator scaling factor for torque (P-AXIS-00325)









Denominator scaling factor for torque (P-AXIS-00326)








Gear couplings








Interpolation of tracked axes in inserted TRC blocks (P-AXIS-00427)








Axis specific dynamic monitoring during interpolation








Suppress stop of spindle axis during channel reset (P-AXIS-00455)








Enabling PLCopen interface of a channel axis (P-AXIS-00457)








Collision monitoring during oscillation (P-AXIS-00485)








Inversion of spindle rotation direction for spindle M-functions M3/M4 (P-AXIS-00490)








Delay filter acts only on command positions (P-AXIS-00513)








Enabling of IPO-LR interface after axis release (P-AXIS-00483)








Setting of 'in position' for position controller generated axis movements (P-AXIS-00458)








Settings for drive controllers








Dynamic limits with tool gear (P-AXIS-00786)








Number of bits for command value (P-AXIS-00816)







Gear step dependent parameters (getriebe[i].*)







Parameters for position control







Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)







Parameters for feedforward control







Parameters for drives (antr.*)







Parameters for manual operation (handbetrieb.*)







Parameters for measurement simulation (meas_simu.*)







Axis-specific filter functions







Parameters for axis specific transformation (trafo.*)







Parameters for path dependent on dynamic weighting (dynamic_weighting.*)







Parameters used by Twincat system manager (twincat.*)







User-defined data (customer.*)







Filter parameters for error handling on axis (error_filter[i].*)







Parameter of the external compensation







Settings for the conveyor tracking functionality (conv_sync.*)







General examples