Overview of axis-specific parameters
Axis data header (kopf.*)
General axis data (kenngr.*)
Functional settings
Special settings for rotary axes
Settings for homing
Settings for software limit switch (SLS) monitoring
Settings for measurement
Activation of edge banding (P-AXIS-00098)
Gantry mode
Monitoring of axis collision
Tracking mode
Gear data
Settings for SAI (Single Axis Interpolation)
Configuration of a SAI-axis (P-AXIS-00250)
Requesting of a SAI axis at RESET (P-AXIS-00251)
Moving to a target position after reversal of direction (P-AXIS-00252)
Switching off superimposed interpolator (P-AXIS-00287)
Synchronising PLCopen axes with exact stop (P-AXIS-00826)
Enable decoupling of the drive of an axis (P-AXIS-00489)
Camming/Gearing (cam_gear.*)
Define axis as Camming / Gearing -Master (P-AXIS-00288)
Velocity tolerance range (P-AXIS-00289)
Minimum time in tolerance range for speed synchronisation (P-AXIS-00290)
Maximum time for velocity synchronisation (P-AXIS-00291)
Average value filter for current master velocity (P-AXIS-00300)
Number of scanning cycles for average value filter (P-AXIS-00301)
Delay time on gearing with current master velocity (P-AXIS-00302)
Maximum commanded velocity for slave axis (P-AXIS-00303)
Maximum commanded acceleration for slave axis (P-AXIS-00304)
Velocity for phase synchronisation (P-AXIS-00305)
Acceleration for phase synchronisation (P-AXIS-00306)
Deceleration for phase synchronisation (P-AXIS-00307)
Jerk for phase synchronisation (P-AXIS-00376)
Jerk for velocity synchronisation (P-AXIS-00377)
Coupling behaviour on error from position control (P-AXIS-00308)
Coupling behaviour on feed enable drop (P-AXIS-00309)
Permissible acceleration of master actual position (P-AXIS-00437)
Error response of the master axis when the coupling is active (P-AXIS-00564)
Error response of the slave axis when the coupling is active (P-AXIS-00565)
Velocity monitoring
Behaviour when enabling the drive controller
Tolerance window for IIR axis filter (P-AXIS-00351)
Tolerance window for IIR axis filter after feedhold (P-AXIS-00780)
Settings for velocity override
Settings for feed rate influencing
Reduced speed
Torque configuration
Gear couplings
Interpolation of tracked axes in inserted TRC blocks (P-AXIS-00427)
Axis specific dynamic monitoring during interpolation
Suppress stop of spindle axis during channel reset (P-AXIS-00455)
Enabling PLCopen interface of a channel axis (P-AXIS-00457)
Collision monitoring during oscillation (P-AXIS-00485)
Inversion of spindle rotation direction for spindle M-functions M3/M4 (P-AXIS-00490)
Delay filter acts only on command positions (P-AXIS-00513)
Enabling of IPO-LR interface after axis release (P-AXIS-00483)
Setting of 'in position' for position controller generated axis movements (P-AXIS-00458)
Settings for drive controllers
Dynamic limits with tool gear (P-AXIS-00786)
Number of bits for command value (P-AXIS-00816)
Gear step dependent parameters (getriebe[i].*)
Parameters for position control
Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)
Parameters for feedforward control
Parameters for drives (antr.*)
Parameters for manual operation (handbetrieb.*)
Parameters for measurement simulation (meas_simu.*)
Axis-specific filter functions
Parameters for axis specific transformation (trafo.*)
Parameters for path dependent on dynamic weighting (dynamic_weighting.*)
Parameters used by Twincat system manager (twincat.*)
User-defined data (customer.*)
Filter parameters for error handling on axis (error_filter[i].*)
Parameter of the external compensation
Settings for the conveyor tracking functionality (conv_sync.*)
General examples