Overview of axis-specific parameters







Axis data header (kopf.*)







General axis data (kenngr.*)







Functional settings








Special settings for rotary axes








Settings for homing









Preferred direction of axis for homing (P-AXIS-00158)









Homing without cam (P-AXIS-00156)









Homing without reverting (P-AXIS-00157)









Position of the reference point (P-AXIS-00152)









Fast velocity for detection of reference cam (P-AXIS-00219)









Slow velocity for exact detection of reference position (P-AXIS-00218)









Homing only with cam (without zero pulse) (P-AXIS-00084)









Slow / fast movement down from cam (P-AXIS-00064)









Maximum velocity for unreferenced axes (P-AXIS-00268)









Lock moving of unreferenced axes (P-AXIS-00277)









Modes for setting the homing position (P-AXIS-00278)









Offset to the homing position (P-AXIS-00279)









Homing method ‘evaluation of encoder overflow’










Selection of the homing method (P-AXIS-00294)










Shifting of encoder overflow (P-AXIS-00354)










Number of bits for evaluation of encoder overflow (P-AXIS-00355)









Acceleration during homing (P-AXIS-00285)









Ramp time during homing (P-AXIS-00286)









Homing type (P-AXIS-00299)









Gantry monitoring during drive-controlled homing (P-AXIS-00298)









Input interface for reference cam signal (P-AXIS-00321)









Use of hardware limit switch as reference switch (P-AXIS-00329)









Maximum distance for zero pulse search (P-AXIS-00404)









Delayed activation of zero pulse logic (P-AXIS-00494)









Maximum distance during homing (P-AXIS-00412)









Maximum distance when moving from reference cam (P-AXIS-00531)









Homing to fixed stop









Reference monitoring (antr.reference_check.*)









Axis remains referenced after resolution change (P-AXIS-00538)









Transfer reference position for drive-controlled homing to the drive (P-AXIS-00584)









Allow drive-controlled homing without controller enable (P-AXIS-00803)









Referencing to limit switch with tracking (P-AXIS-00814)








Settings for software limit switch (SLS) monitoring








Settings for measurement








Activation of edge banding (P-AXIS-00098)








Gantry mode








Monitoring of axis collision








Tracking mode








Gear data








Settings for SAI (Single Axis Interpolation)








Velocity monitoring








Behaviour when enabling the drive controller








Tolerance window for IIR axis filter (P-AXIS-00351)








Tolerance window for IIR axis filter after feedhold (P-AXIS-00780)








Settings for velocity override








Settings for feed rate influencing








Reduced speed








Torque configuration








Gear couplings








Interpolation of tracked axes in inserted TRC blocks (P-AXIS-00427)








Axis specific dynamic monitoring during interpolation








Suppress stop of spindle axis during channel reset (P-AXIS-00455)








Enabling PLCopen interface of a channel axis (P-AXIS-00457)








Collision monitoring during oscillation (P-AXIS-00485)








Inversion of spindle rotation direction for spindle M-functions M3/M4 (P-AXIS-00490)








Delay filter acts only on command positions (P-AXIS-00513)








Enabling of IPO-LR interface after axis release (P-AXIS-00483)








Setting of 'in position' for position controller generated axis movements (P-AXIS-00458)








Settings for drive controllers








Dynamic limits with tool gear (P-AXIS-00786)








Number of bits for command value (P-AXIS-00816)







Gear step dependent parameters (getriebe[i].*)







Parameters for position control







Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)







Parameters for feedforward control







Parameters for drives (antr.*)







Parameters for manual operation (handbetrieb.*)







Parameters for measurement simulation (meas_simu.*)







Axis-specific filter functions







Parameters for axis specific transformation (trafo.*)







Parameters for path dependent on dynamic weighting (dynamic_weighting.*)







Parameters used by Twincat system manager (twincat.*)







User-defined data (customer.*)







Filter parameters for error handling on axis (error_filter[i].*)







Parameter of the external compensation







Settings for the conveyor tracking functionality (conv_sync.*)







General examples