Overview of axis-specific parameters
Axis data header (kopf.*)
General axis data (kenngr.*)
Functional settings
Special settings for rotary axes
Settings for homing
Settings for software limit switch (SLS) monitoring
Settings for measurement
Activation of edge banding (P-AXIS-00098)
Gantry mode
Axis number of master axis (P-AXIS-00070)
Resettable path distance (P-AXIS-00072)
Non resettable path distance (P-AXIS-00071)
Static offset (P-AXIS-00073)
Velocity of correction (P-AXIS-00075)
Gantry difference monitoring before homing (P-AXIS-00249)
Drive-controlled homing of gantry axis (SERCOS) (P-AXIS-00253)
CNC-controlled error reaction (P-AXIS-00254)
Conditions for clearing the gantry difference (P-AXIS-00704)
Maximum path for a gantry slave axis during homing (P-AXIS-00284)
Suppress homing for gantry slave axis (P-AXIS-00074)
Home gantry slave axis relative to encoder overflow (P-AXIS-00393)
Behaviour on setting the homing position (P-AXIS-00445)
Edge detection GantryOn-signal (P-AXIS-00261)
Monitoring of axis collision
Tracking mode
Gear data
Settings for SAI (Single Axis Interpolation)
Velocity monitoring
Behaviour when enabling the drive controller
Tolerance window for IIR axis filter (P-AXIS-00351)
Tolerance window for IIR axis filter after feedhold (P-AXIS-00780)
Settings for velocity override
Settings for feed rate influencing
Reduced speed
Torque configuration
Gear couplings
Interpolation of tracked axes in inserted TRC blocks (P-AXIS-00427)
Axis specific dynamic monitoring during interpolation
Suppress stop of spindle axis during channel reset (P-AXIS-00455)
Enabling PLCopen interface of a channel axis (P-AXIS-00457)
Collision monitoring during oscillation (P-AXIS-00485)
Inversion of spindle rotation direction for spindle M-functions M3/M4 (P-AXIS-00490)
Delay filter acts only on command positions (P-AXIS-00513)
Enabling of IPO-LR interface after axis release (P-AXIS-00483)
Setting of 'in position' for position controller generated axis movements (P-AXIS-00458)
Settings for drive controllers
Dynamic limits with tool gear (P-AXIS-00786)
Number of bits for command value (P-AXIS-00816)
Gear step dependent parameters (getriebe[i].*)
Parameters for position control
Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)
Parameters for feedforward control
Parameters for drives (antr.*)
Parameters for manual operation (handbetrieb.*)
Parameters for measurement simulation (meas_simu.*)
Axis-specific filter functions
Parameters for axis specific transformation (trafo.*)
Parameters for path dependent on dynamic weighting (dynamic_weighting.*)
Parameters used by Twincat system manager (twincat.*)
User-defined data (customer.*)
Filter parameters for error handling on axis (error_filter[i].*)
Parameter of the external compensation
Settings for the conveyor tracking functionality (conv_sync.*)
General examples