Overview of axis-specific parameters
Axis data header (kopf.*)
General axis data (kenngr.*)
Functional settings
Gear step dependent parameters (getriebe[i].*)
Parameters for position control
Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)
Parameters for feedforward control
Parameters for drives (antr.*)
Parameters for manual operation (handbetrieb.*)
Parameters for measurement simulation (meas_simu.*)
Axis-specific filter functions
Parameters for axis specific transformation (trafo.*)
Parameters for path dependent on dynamic weighting (dynamic_weighting.*)
Parameters used by Twincat system manager (twincat.*)
User-defined data (customer.*)
Filter parameters for error handling on axis (error_filter[i].*)
Parameter of the external compensation
Settings for the conveyor tracking functionality (conv_sync.*)
Definition of the conveyor axis (P-AXIS-00708)
Actual position value filter for the conveyor axis (P-AXIS-00620)
Order of the actual speed value filter of the conveyor axis (P-AXIS-00623)
Order of the downstream velocity actual value filter in the case of feedhold on the conveyor axis (P-AXIS-00624)
Order of the actual speed filter in the case of feedhold on the conveyor axis (P-AXIS-00625)
Delay time between the latch moment of the actual values and generating the command value P-AXIS-00626)
Method to monitor the workspace with conveyor tracking (P-AXIS-00555)
General examples