Overview of axis-specific parameters
Axis data header (kopf.*)
General axis data (kenngr.*)
Functional settings
Special settings for rotary axes
Settings for homing
Preferred direction of axis for homing (P-AXIS-00158)
Homing without cam (P-AXIS-00156)
Homing without reverting (P-AXIS-00157)
Position of the reference point (P-AXIS-00152)
Fast velocity for detection of reference cam (P-AXIS-00219)
Slow velocity for exact detection of reference position (P-AXIS-00218)
Homing only with cam (without zero pulse) (P-AXIS-00084)
Slow / fast movement down from cam (P-AXIS-00064)
Maximum velocity for unreferenced axes (P-AXIS-00268)
Lock moving of unreferenced axes (P-AXIS-00277)
Modes for setting the homing position (P-AXIS-00278)
Offset to the homing position (P-AXIS-00279)
Homing method ‘evaluation of encoder overflow’
Acceleration during homing (P-AXIS-00285)
Ramp time during homing (P-AXIS-00286)
Homing type (P-AXIS-00299)
Gantry monitoring during drive-controlled homing (P-AXIS-00298)
Input interface for reference cam signal (P-AXIS-00321)
Use of hardware limit switch as reference switch (P-AXIS-00329)
Maximum distance for zero pulse search (P-AXIS-00404)
Delayed activation of zero pulse logic (P-AXIS-00494)
Maximum distance during homing (P-AXIS-00412)
Maximum distance when moving from reference cam (P-AXIS-00531)
Homing to fixed stop
Velocity (P-AXIS-00333)
Acceleration (P-AXIS-00334)
Jerk (P-AXIS-00335)
Minimum distance (P-AXIS-00344)
Maximum distance (P-AXIS-00345)
Direction (P-AXIS-00346)
Velocity limit value (P-AXIS-00347)
Retraction distance (P-AXIS-00348)
Reference position (P-AXIS-00349)
Minimum time (P-AXIS-00350)
Position lag limit for fixed stop detection when homing to a fixed stop (P-AXIS-00819)
Residual torque to detect a fixed stop during homing to a fixed stop (P-AXIS-00820)
Distance to fixed stop for simulation (P-AXIS-00822)
Reference monitoring (antr.reference_check.*)
Axis remains referenced after resolution change (P-AXIS-00538)
Transfer reference position for drive-controlled homing to the drive (P-AXIS-00584)
Allow drive-controlled homing without controller enable (P-AXIS-00803)
Referencing to limit switch with tracking (P-AXIS-00814)
Settings for software limit switch (SLS) monitoring
Settings for measurement
Activation of edge banding (P-AXIS-00098)
Gantry mode
Monitoring of axis collision
Tracking mode
Gear data
Settings for SAI (Single Axis Interpolation)
Velocity monitoring
Behaviour when enabling the drive controller
Tolerance window for IIR axis filter (P-AXIS-00351)
Tolerance window for IIR axis filter after feedhold (P-AXIS-00780)
Settings for velocity override
Settings for feed rate influencing
Reduced speed
Torque configuration
Gear couplings
Interpolation of tracked axes in inserted TRC blocks (P-AXIS-00427)
Axis specific dynamic monitoring during interpolation
Suppress stop of spindle axis during channel reset (P-AXIS-00455)
Enabling PLCopen interface of a channel axis (P-AXIS-00457)
Collision monitoring during oscillation (P-AXIS-00485)
Inversion of spindle rotation direction for spindle M-functions M3/M4 (P-AXIS-00490)
Delay filter acts only on command positions (P-AXIS-00513)
Enabling of IPO-LR interface after axis release (P-AXIS-00483)
Setting of 'in position' for position controller generated axis movements (P-AXIS-00458)
Settings for drive controllers
Dynamic limits with tool gear (P-AXIS-00786)
Number of bits for command value (P-AXIS-00816)
Gear step dependent parameters (getriebe[i].*)
Parameters for position control
Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)
Parameters for feedforward control
Parameters for drives (antr.*)
Parameters for manual operation (handbetrieb.*)
Parameters for measurement simulation (meas_simu.*)
Axis-specific filter functions
Parameters for axis specific transformation (trafo.*)
Parameters for path dependent on dynamic weighting (dynamic_weighting.*)
Parameters used by Twincat system manager (twincat.*)
User-defined data (customer.*)
Filter parameters for error handling on axis (error_filter[i].*)
Parameter of the external compensation
Settings for the conveyor tracking functionality (conv_sync.*)
General examples