Overview of axis-specific parameters
Axis data header (kopf.*)
General axis data (kenngr.*)
Functional settings
Special settings for rotary axes
Settings for homing
Settings for software limit switch (SLS) monitoring
Settings for measurement
Define axis as measurement axis (P-AXIS-00118)
Probe stroke for measurement types 2 and 4 (P-AXIS-00086)
Measurement speed for measurement type 2 (P-AXIS-00215)
Measurement travel offset for measurement type 2 (P-AXIS-00114)
Measurement travel offset for all measurement types (P-AXIS-00467)
Measurement signal parameters (kenngr.measure.*)
Measurement parameters for SERCOS drives
Parameters for measuring travel on fixed stop
Limit for position lag (P-AXIS-00331)
Number of position control cycles (P-AXIS-00332)
Position lag limit for fixed stop detection when measuring travel on fixed stop (P-AXIS-00774)
Minimum time for fixed stop detection when measuring travel on fixed stop (P-AXIS-00775)
Minimum path to activate fixed stop detection when measuring travel on fixed stop (P-AXIS-00776)
Percentage minimum path for fixed stop detection when measuring travel on fixed stop (P-AXIS-00777)
Maximum position change for fixed stop detection when measuring travel on fixed stop (P-AXIS-00778)
Slave axes to detect a fixed stop during Measuring travel to fixed stop (P-AXIS-00835)
Abortion of measuring order at reset (P-AXIS-00378)
Actuation time delay of probe (P-AXIS-00487)
Activation of edge banding (P-AXIS-00098)
Gantry mode
Monitoring of axis collision
Tracking mode
Gear data
Settings for SAI (Single Axis Interpolation)
Velocity monitoring
Behaviour when enabling the drive controller
Tolerance window for IIR axis filter (P-AXIS-00351)
Tolerance window for IIR axis filter after feedhold (P-AXIS-00780)
Settings for velocity override
Settings for feed rate influencing
Reduced speed
Torque configuration
Gear couplings
Interpolation of tracked axes in inserted TRC blocks (P-AXIS-00427)
Axis specific dynamic monitoring during interpolation
Suppress stop of spindle axis during channel reset (P-AXIS-00455)
Enabling PLCopen interface of a channel axis (P-AXIS-00457)
Collision monitoring during oscillation (P-AXIS-00485)
Inversion of spindle rotation direction for spindle M-functions M3/M4 (P-AXIS-00490)
Delay filter acts only on command positions (P-AXIS-00513)
Enabling of IPO-LR interface after axis release (P-AXIS-00483)
Setting of 'in position' for position controller generated axis movements (P-AXIS-00458)
Settings for drive controllers
Dynamic limits with tool gear (P-AXIS-00786)
Number of bits for command value (P-AXIS-00816)
Gear step dependent parameters (getriebe[i].*)
Parameters for position control
Parameters of the axis peripheral interfaces for position control (lr_hw[i].*)
Parameters for feedforward control
Parameters for drives (antr.*)
Parameters for manual operation (handbetrieb.*)
Parameters for measurement simulation (meas_simu.*)
Axis-specific filter functions
Parameters for axis specific transformation (trafo.*)
Parameters for path dependent on dynamic weighting (dynamic_weighting.*)
Parameters used by Twincat system manager (twincat.*)
User-defined data (customer.*)
Filter parameters for error handling on axis (error_filter[i].*)
Parameter of the external compensation
Settings for the conveyor tracking functionality (conv_sync.*)
General examples