TwinCAT System Manager: System - Configuration |
At the SYSTEM - Configuration tree-entry, project-specific TwinCAT System- and Real-Time Settings can be made.
User-defined Tasks can also be created, e.g. to output or read I/O device values from high-level language applications (Visual Basic-, Visual C++, C# .NET, Visual Basic.NET or Delphi).
SYSTEM - Configuration | Description |
---|---|
Boot Settings | Boot / Auto-Logon settings for the local and for the target system |
Real-Time Settings | Configuration of TwinCAT Real-Time settings and display for Real-Time load |
Priorities | Display / manipulation (= Advanced User) of TwinCAT Task priorities |
User-defined Tasks ("Additional Tasks") | Configuration of possible additional user-defined tasks |
Task settings for "Additional Tasks" (if configured) | Dialog for settings of user-defined tasks |
Online Display Task Load (if additional user-defined tasks are configured) | Online view for the load of the user-defined task |
Task Process Images (if additional user-defined tasks are configured) | Mapping informations about user-defined tasks |
Route Settings | Informations about TwinCAT target system routing |
This dialog only appears, if no Remote system is selected, means the System Manager accesses the local target system (see also "Choose Target System").
Besides that, the following dialog "Version [Local]" is equivalent.
The following dialog shows the installed TwinCAT Level of the lokale system (at this example it is "TwinCAT NC I" ) and the version und "Build"- number of it (correspondingly the version 2.9 [Build 931]).
Besides the info about the locally installed TwinCAT version, another tab with corresponding info about the selected TwinCAT target system is available. The following dialog shows e.g. version 2.9 [Build 0].
Choose Target: Calls the selection dialog for TwinCAT target systems, accessible by TwinCAT Router. See also: Main Menus -> "Actions"