TwinCAT System Manager: NC Configuration

Overview

If TwinCAT is installed with NC function capability (minimum: TwinCAT Level  NC PTP) you will see "NC Configuration" in the tree view of the System Manager. Here you can create the required axes and set their parameters. When TwinCAT  is started, it's also possible to drive axes via corresponding online dialogues (NC Manual Menu, Online Display of Axis Channel)  and carry out other NC axis functions like manual coupling etc..).

 

NC - Configuration Description
Tasks NC task settings
Channel Information about axis channel
Axes Configuration of individual axes
Cam Design Configuration of Cam plates with TwinCAT Cam Design Tool 
Hydraulic Valve Diagrams Configuration of special characteristics for hydraulic valves with TwinCAT Valve Diagram Editor  

 

"General" Tab

This dialog only appears, if no Remote system is selected, means the System Manager accesses the local target system (see also  "Choose Target System").
Besides that, the following dialog "Version [Target]" is equivalent.

 

Dialog "Version [Target]"

The following dialog describes the TwinCAT server of the target system, where this module is based on. In the shown dialog this is the - currently active - version 2.9 [Build 531] of the TwinCAT NC Server.

Overview 1: