TwinCAT System Manager: I/O - Configuration |
The I/O - Configuration is an important component of the TwinCAT System Manager. The lowest level of TwinCAT is TwinCAT Level I/O, means an I/O Configuration entry in the TwinCAT System Manager tree- view is always present. After the various Configurations have been executed for the different tasks and the System Manager has been acquainted with all relevant variables, the hardware (usually a fieldbus with I/O modules) is configured under this rubric. It is also possible to configure the I/O section first and the other tasks (e.g. PLC tasks) later on, of course.
I/O - Configuration | Description |
---|---|
I/O Devices | At target system (local or remote) configured Input and Output devices (Fieldbus cards, NOVRAM, system interfaces,..) and their process images |
Mappings | Informations about mappings between the I/O devices and other TwinCAT devices, resp. their process images |
This dialog only appears, if no Remote system is selected, means the System Manager accesses the local target system (see also "Choose Target System").
Besides that, the following dialog "Version [Target]" is equivalent.
The following dialog describes the TwinCAT server of the target system, where this module is based on. In the shown dialog this is the - currently active - version 2.9 [Build 418] of the TwinCAT IO Server.