TwinCAT System Manager: NC Configuration |
If TwinCAT is installed with NC function capability (minimum: TwinCAT Level NC PTP) you will see "NC Configuration" in the tree view of the System Manager. Here you can create the required axes and set their parameters. When TwinCAT is started, it's also possible to drive axes via corresponding online dialogues (NC Manual Menu, Online Display of Axis Channel) and carry out other NC axis functions like manual coupling etc..).
NC - Configuration | Description |
---|---|
Tasks | NC task settings |
Channel | Information about axis channel |
Axes | Configuration of individual axes |
Cam Design | Configuration of Cam plates with TwinCAT Cam Design Tool |
Hydraulic Valve Diagrams | Configuration of special characteristics for hydraulic valves with TwinCAT Valve Diagram Editor |
This dialog only appears, if no Remote system is selected, means the System Manager accesses the local target system (see also "Choose Target System").
Besides that, the following dialog "Version [Target]" is equivalent.
The following dialog describes the TwinCAT server of the target system, where this module is based on. In the shown dialog this is the - currently active - version 2.9 [Build 531] of the TwinCAT NC Server.