TwinCAT System Manager: Variable Links

Variable Links

The various task input or output variables can be linked when selected either with the context menu or the dialogue shown on the right-hand side, e.g. with the I/O Configuration.

Context Menu

Some of the selection options in the context menu are only available when the configuration is active and the system is running or they have other dependencies. If that is the case, they aren't high-lighted.

Variable Links 1:

 

Change Link

Opens the Selection Dialog for determining the target variable to be linked.

Clear Link(s)

Removes a link (indicated with a small arrow to the left of the variable symbol) from a variable.

Goto Link Variable

Jumps to the linked target variable (e.g. Bus Terminal channel or in/output variable of another task) in the System Manager tree.

Insert Variable

Adds further variables to the task (do not use for PLC tasks as these variables should be specified within the PLC project).

Delete

Deletes corresponding variable from the list.

Move Address

Moves the address of the marked variable within the Process Image.

Online Write

Overwrites the current variable value with a user-defined value for one cycle.

Online Force 

Overwrites the current variable value with a user-defined value until halted using Cancel Force.

Release Force

Cancels forced variable and restores the actual variable value.

Add to Watch

Adds the selected variable to the Watch Window. You can carry out a continuous observation of the current online variable values.

Remove from Watch

Deletes the selected variable from the Watch window

Create Linked Variable in

Adds linked variable to an existing PLC project.