BECKHOFF BX Controler: Appendix

Example Programs - Overview

Denomination Description
Display Example for controlling the display
Navigation switch Reading of the navigation switch from the PLC
Menu Example for own menu with navigation switch and display
COM port - BK/BC8x00 Master Interface COM 1 or COM 2 interface as a master with the BK8x00 protocol
COM port - BK8x00 Slave Interface COM 1 or COM 2 interface as a slave with the BK8x00 protocol
COM port - Cimrex 12 Example for controlling a CIMREX 12 display via ModbusRTU
COM port - ModbusRTU Slave Link of ModbusRTU Lib with the COM 1 or COM 2 interface of the BX
COM port - ModbusRTU Master Link of ModbusRTU Lib with the COM 1 or COM 2 interface of the BX
COM port - RK512 Protocol RK512 protocol via COM 1 or COM 2
COM port - ComLibV2 Example with COMlibV2m, send strings
RTC Example for reading the RTC via function blocks
SMS via COM port Connecting an Siemens S35 mobile phone via the COM interface for sending SMS messages
SSB - Display Cimrex panel at SSB
SSB - AX2000 AX2000 at SSB
SSB - BK51x0 BK5120 at SSB
SSB - BX / BX communication Communication from BX to BX (via SSB)
SSB - IclA Drive IclA Drive at SSB
SSB - Lenze Drive Lenze Frequency Converter at SSB