TwinCAT 3 PLC

ROR

IEC operator: Bitwise rotation of an operand to the right.

erg = ROR (in, n)

Allowed data types: BYTE, WORD, DWORD, LWORD.

in will be shifted one bit position to the right n times while the bit that is furthest to the left will be reinserted from the left.

Note_A4

NOTICE!

Please note, that the amount of bits, which is noticed for the arithmetic operation, is pretended by the data type of the input variable ! If the input variable is a constant the smallest possible data type is noticed. The data type of the output variable has no effect at all on the arithmetic operation.

See in the following example in hexadecimal notation that you get different results for erg_byte and erg_word depending on the data type of the input variable (BYTE or WORD), although the values of the input variables in_byte and in_word are the same.

Example in ST:

PROGRAM ror_st

VAR

in_byte : BYTE:=16#45;

in_word : WORD:=16#45;

erg_byte : BYTE;

erg_word : WORD;

n: BYTE :=2;

END_VAR

erg_byte:=ROR(in_byte,n); (* Result is 16#51 *)

erg_word:=ROR(in_word,n); (* Result is 16#4011 *)

Example in FBD:

Example in IL: